Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

lock attach
Attachments are accessible only for community members.
hata_3396041
Level 4
Level 4
First solution authored First like received 50 questions asked

Hi

Try to drive the LCD with the PSoC4 MCU.

An example post of driving a 1/3 DUTY 1 / 2BIAS 3com x18 seg LCD using PSoC 4100S (CY8C4146LQI-S433).

Tools

LCD(HD18253T)

hata_3396041_0-1648694929277.png

 

PSoC4(CY8C4146LQI-S433)

Use the following as the board of CY8C4146LQI-S433.

hata_3396041_1-1648695008772.png

 

 

Connection, verification

Use the above tools to connect the PSoC 4 MCU to the LCD.

hata_3396041_3-1648693506211.png

The details of the connection are shown below.

hata_3396041_4-1648693563718.png

The LCD consists of 4 7 segments and 15 Bars.

LCD display communicates with EZI2C and is controlled from the Bridge Control Panel of the PC.

Attach the HD18253T.iic file.

hata_3396041_5-1648693640838.pnghata_3396041_6-1648693736307.png

 

If you select all the Editor screens of the Bridge Control Panel and click "Repeat", the weight of 500ms is inserted, so the display will be updated at 500ms intervals.

hata_3396041_7-1648693853911.png

The PSoC4100S controls the LCD by PWM. Please refer to AN87391

AN87391 

 

Best Regards

Haya

 

 

 

 

 

 

 

 

 

 

 

0 Replies