- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am uploading v1.0 of the KIT-059 annotation component. It is made as a stand-alone component for those who doesn't need the entire Annotation Library.
The KIT-059 is an external annotation stub for the Cypress CY8CKIT-059 PSoC 5LP Prototyping Kit. It was developed to assist quick identification of the on-board components and pins on the CY8CKIT-059 PSoC 5LP Prototyping Kit.
The KIT-059 annotation component can be used in conjunction with small-sized annotation components from Annotation Library, as well as Cypress stock annotation components (capacitors, resistors, etc.)
Attached archive contains KIT-059 component library, a Datasheet and installation instructions. Upon installation it will show up in the folder:
/Community/Off-Chip/Annotation Library/Kits/
The component provided as-is, no liabilities. It is free to use, modify and distribute.
regards,
odissey1
Figure 1. Component appearance by options selected: (a) all options enabled, (b) default appearance, (c) only misc. options enabled, (d) all options disabled
Figure 2. Component appearance by the group of options selected: (a) bypass capacitors, (b) OpAmps, (c) DACs, (d) SAR_ADCs external reference.
Figure 3. Schematic example using KIT-059 (v1.0) and Annotation Library (v1.0)
(11/27/2019) message was edited by odissey1 - cosmetic update of the Opamp3 visual appearance in the follower mode.
- Labels:
-
ispn:39618:1:0
-
l1:314:1:0
-
PSoC345LP
- Tags:
- annotation
- annotation component
- annotation library
- community component
- cy8ckit-059
- cypress
- kit-059
- library
- odissey1
- prototyping kit
- psoc5
- psoc5lp