- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Here I am uploading annotation component for the CY8CKIT-044 PSoC4 M-series Pioneer Kit
The KIT-044 component shows pins with direct connection to the ADC_SAR bypass capacitor, OpAmps, I2C, UART, RGB LEDs, light and temperature sensors, accelerometer and FRAM. The component helps to visualize ports and pins and helps create connection diagrams for CY8CKIT-044 Pioneer Kit.
The KIT-044 annotation component can be used in conjunction with small-sized annotation components from PSoC Annotation Library, as well as Cypress stock annotation components (capacitors, resistors, etc.)
Attached archive contains KIT-044 component library. Upon installation it will show up in the folder:
/Community/Off-Chip/Annotation Library/Kits/
The component provided as-is, no liabilities. It is free to use, modify and distribute.
regards,
/odissey1
Message was edited by: odissey1 Changed link to a new version of the PSoC Annotation Library v1.0
- Labels:
-
ispn:39614:1:0
-
l1:314:1:0
-
PSoC345LP
- Tags:
- annotation
- annotation component
- annotation libraty
- community component
- cy8ckit-044
- cy8kit-044
- cypress
- kit-044
- kit-044m
- library
- m-series
- odissey1
- off-chip
- pioneer board
- pioneer kit
- psoc4200m
- psoc4m
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
Attached below is new updated version (v0.2) of the KIT-044 component.
Changes include:
1. The component Datasheet is provided.
2. Pins are re-aligned to match the standard Arduino layout
3. Added I2C pullup resistors on pins 4.0 and 4.1.
4. Opamp1 inputs are moved to the buried pins.
5. Minor cosmetic enhancements (added colors to RGB LEDs, etc.).
/odissey1
Fig. 1. KIT-044 (v0.2) with all visual options enabled.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear /odissey1-san,
Nice update!
I like the new "config" function!
BTW, will it bother you to ask if we can have UART_RX instead of RX and UART_TX instead of TX?
I searched UART and finally found it because of the P7[0] and P7[1].
May be it is only I, who can not map UART_RX/UART_TX to RX/TX instantly though.
Best Regards,
26-Sep-2019
Motoo Tanaka
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Moto,
Thank you for reviewing the component and valuable suggestion. I updated component and the datasheet above, in order not to create a new version. Hope it will be useful for you.
Sincerely,
/odissey1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear /odissey1-san,
Thank you very much for your quick update!
My test project could be updated by only replacing the KIT-044_lib folder.
Yes, I'm very happy with this 😉
Best Regards,
26-Sep-2019
Motoo Tanaka