Attachments are accessible only for community members.
Nov 29, 2020
02:13 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 29, 2020
02:13 PM
Hi all,
I make a CE which I2S in PSoC6 for CM4. This is a loopback program that divides data into two buffer for L / R using DMA.
The environment used is as follows:
・PSoC Creator 4.4
・CY8CKIT-062-BLE
・I2S format: 24bit 2word 1bit Delay
The array data of Tx or Rx is divided in half. The upper part is L and the lower part is R.
DMA Settings:
For Tx
For Rx
The circuit:
The observed waves and Rx Buffer values:
Thanks,
Kenshow
Labels
- Labels:
-
PSoC 6
0 Replies