Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

Provided below are custom 16-bit Control and Status Register components (ControlReg16 and StatusReg16). They allow firmware write to and read from up to 16 digital signals simultaneously.

Component features:
     up to 16-bit firmware read/write access
     16-bit DMA access

The components were designed exclusively for PSoC5 with 24 UDB cells, and tested using CY8KIT-059 PSoC5LP Prototyping Kit.  Demo projects are provided.

Attached archive contains components library, component datasheets and demo projects for PSoC5LP. Please read installation instructions in the readme.txt.

The component provided as-is, no liabilities. It is free to use and modify.
/odissey1

Figure 1. Typical use of the ControlReg16 and StatusReg16 for sampling and setting digital ports. 

CReg16-SReg16_example_A.png

 

Figure 2. Example of the 16-bit DMA transfer from the RAM Buffer to the ControlReg16.

RAM-DMA-CReg16_01b_A.png

 

Figure 3. Example of the 16-bit DMA transfer from the StatusReg16 to the RAM Buffer.

Sreg16-DMA-RAM_01b_A.png

1 Reply
jepaz
Level 4
Level 4
25 replies posted 10 replies posted 10 questions asked

This Looks really useful will give it a try! thank you for sharing!! awesome work!

0 Likes