- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am uploading a library of small off-chip components for annotation of the CY8CKIT-059 PSoC 5LP Prototyping Kit.
The KIT-059 component shows all on-board capacitors and pins with direct connections to the OpAmps, DACs, SARs, I2C, UART, LED and XTAL. It helps visualizing ports and pins and making connection diagrams for CY8CKIT-059 Prototyping Kit.
The accompanying library contains few small-sized off-chip annotation components (resistor, capacitors, OpAmps, DAC, etc.). The components are about 50% smaller than their stock analogs, allowing for tighter schematic placement.
The demo project shows all-analog PID control of the levitationg globe, implemented in CY8CKIT-059 PSoC 5LP Prototyping Kit, with annotation diagram created using KIT-059 component.
Attached archive contains component library, a demo project and enlarged picture of the Prototyping Kit. Last tested under Creator 3.3 CP3.
regards,
odissey1
//==============================================================================================
// ANNOUNCEMENT
//
//==============================================================================================
New version of the Annotation Library (v1.0) is available for download in the Community Code Examples section:
Please note that the Library structure has been re-worked entirely, so that old components (Resistor, Capacitor, etc. will not upgrade). The KIT-059 will update OK.
I recommend to use v1.0 of the Library for new projects, while keeping old projects as-is.
Message was edited by: odissey1 (Aug 01, 2019)
- Labels:
-
ispn:39618:1:0
-
l1:314:1:0
-
PSoC345LP
- Tags:
- annotation
- annotation library
- community component
- custom component
- kit-059
- library
- odissey1
- off-chip
- psoc5 kit