Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Code Examples

Len_CONSULTRON
Level 9
1000 replies posted 750 replies posted 500 likes received
Level 9

I've attached a custom component that is a TopDesign selectable component for the PSoC5 LPF (low-pass filter) block.

Previously the 2 fixed function LPF blocks available in the PSoC5 were only available by accessing the PSoC5 registers directly.   With this component, it can be included, configured (4 corner frequency selections) and routed by PSoC Creator.

This component has a number of run-time APIs to allow for setting a "new" corner frequency and to stop or disable it.

If the component is Stopped or Disabled, the LPF will automatically BYPASS to allow the full frequency spectrum of the input to the output.  Re-enabling or starting the LPF will invoke the last corner frequency setting.

Requirements:

  • PSoC Creator 4.2 or higher.
  • PSoC5 Device Family.

Enjoy,

Len

Len
"Engineering is an Art. The Art of Compromise."
1 Reply
JeetendraA_51
Moderator
Moderator 10 replies posted 5 replies posted First reply posted
Moderator

Thank you Len for sharing the custom component!

0 Likes