Dec 08, 2021
02:55 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dec 08, 2021
02:55 AM
Hi,
In the following discussion,
I was asked for a sample to emulate an Arduino sample below
https://www.youtube.com/watch?v=DuAG98P9Seo
Unlike the Arduino sample, I used a non-I2C LCD 1602A.
Also I prepared a simple menu system which can be expanded later (hopefully) without modifying the main loop.
void do_menu_1(void) ;
void do_menu_2(void) ;
void do_menu_3(void) ;
void do_menu_4(void) ;
m_list_type menu[] = {
{ "MenuItem1", do_menu_1, "first menu" },
{ "MenuItem2", do_menu_2, "second menu" },
{ "MenuItem3", do_menu_3, "third menu" },
{ "MenuItem4", do_menu_4, "fouth menu" }
} ;
int num_menu = sizeof(menu) / sizeof(m_list_type) ;
int current_menu_row = 0 ;
int active_menu_id = 0 ;
int menu_height = 2 ;
For the operation, I mapped
C: up
😧 down
#: select
Matrix Key Schematic
CharLCD Schematic
For the CharLCD (1602A), the only pin combination, I could find to be usable were P2[6:0] or P2[7:1].
And with this configuration, CY8CKIT-059's LED and push-SW won't be usable for other purpose.
And finally I noticed the A pin of 1602A can be used for backlight ... >_<
Anyway, here it is.
moto
Labels
- Labels:
-
CharLCD
-
CY8CKIT-059
-
Matrix Key
-
PSoC 5LP
0 Replies