Clocks Forum Discussions
At lower temperature, transistors become faster, so edge rates would become faster.
Generally, we would expect the following parameters getting affected as temperature decreases beyond the specified operating limit:
1) Decreased frequency operating range (for reliable locking)
2) Faster edge rates
3) Higher jitter
4) Duty Cycle
Operating a device outside of its design range is very risky. While it is possible that the only effects of operating at a reduced temperature will be shifts to some parameters such as duty cycle and edge rates, it is also possible that the device performance may degrade more seriously. It may also fail to operate reliably. For example, the PLL may not lock or may lose lock, or the spread profile in case of spread aware buffers could become much distorted.
Show LessUsually the CY2308 is not designed as a Fail Safe device. However, the PLL of the 2308 will not lose lock as a consequence of the oscillator being pulled by a few hundred PPM. The 2308 PLL will be able to track any low frequency variations in the reference input and will filter out any high frequency variations greater than the loop bandwidth which is around 1 to 2 MHz, typically 1.5 MHz.
Cypress System Engineers have tested this glitch operation for different reference frequencies: 33MHz, 66 MHz, 100 MHz, and 133MHz. The signal at the PLL output remained for the minimum of 2.3uSec after the input signal was shut off. This free running output frequency drifted slowly but no glitch was observed in any case. The measurement was under 3.3V power supply room temperature. So accordingly, it would not lose lock with a single glitch.
Show Less
Usually the Propagation delay, Duty Cycle, Rise and fall time values increase with increase in temperature when you go beyond the temperature grade rating for a Commercial and Industrial grade device. At higher temperatures your transistors will switch slower and your jitter will go up. If you increase your drive strength it may help to reduce jitter since you will have slightly faster edges.
Generally the device is not characterized beyond the Industrial temperature range for an Industrial grade device and therefore the specifications like jitter or duty cycle cannot be guaranteed when the temperature range is exceeded. There are chances that the device may run in locking and reliability issues when the temperature range is exceeded and especially when you are working at the higher maximum frequencies. Usually the maximum frequency range is decreased for Industrial temperature grade as compared to commercial temperature grade that can be seen in the respective datasheet.
Show LessCurrently Cypress does not have much buffer devices in the lower MHz range or KHz range. There is CY2302 amongst zero delay buffers that can go down to 5MHz.
Most of the zero delay buffers have a minimum input frequency of 10MHz. So operation with input reference below 10MHz minimum of the device cannot be guaranteed. If a PLL operates near the point of instability, the PLL lock time can become excessive.
10 Mhz is a guard band of the minimum frequency. When this frequency is reached, the zero delay buffers usually will go into power down mode as it would when there is no input. There is no guarantee on any other specifications likes duty cycle, jitter, lock times etc. when the input frequency specification range is violated at the lower end.
Show LessEven if there is no ripple at the supply source, you will see ripple at the Vdd pin of a Buffer when its outputs are switching. The switching outputs create large di/dt which causes Vdd and Vss noise both inside the chip and externally. That is why the external decoupling is so important, because only local capacitors are capable of servicing those large current transients. Also, inductance on Vss and Vdd must be minimized. When a ferrite bead is added to the Vdd path, it increases the Vdd path inductance. This is good for EMI, but it makes it that much more important that very good decoupling be provided between the ferrite and the chip.
If still some incorrect oscillation is happening, it is likely that the poor VDD layout is playing a major roll in the problem. The VDD trace to the nearest capacitor should not be very narrow and should not be long with a Via. It’s always recommended that decoupling capacitors be placed as close as possible to the VDD pin, and that it is connect to the pin with a wide trace. So most of the VDD noise comes from the device itself, due to the multiple outputs switching, which makes good decoupling very important.
Check for more details the following chapters of Perfect Timing II book available at: http://www.cypress.com/?rID=98
Chapter 5 – Power Supply Filtering
Chapter 6 – PCB Layout Considerations
Chapter 8 – Bypass Capacitors
Show LessTips to minimize output-output skew are as follows:
1. Keep same length transmission lines at output.
2. Allow only one frequency output simultaneously.
3. Use same Vdd on all output buffers.
4. Terminate outputs in same way; use sufficient bypass capacitors.
5. For devices in parallel, feed inputs same ref clock in most symmetrical way possible.
6. Route outputs in most symmetrical way possible.
The goal of any frequency synthesizer is to generate a desired output frequency based on a given input reference frequency. However, this relationship between available input frequency and required output frequency is not always obvious. The question always looms: Is there another, better configuration for my PLL that will deliver better noise performance and lower power? Read more of this article at EE Times.
Show LessMaking a choice to go for ZDB (Zero Delay Buffer) or NZDB (Non-Zero Delay Buffer) is fairly dependent on your application requirements.
With ZDB, we have a PLL inside that gives zero delay between input and output. This filters jitter present at the reference and has less jitter at the output in ps (Jitter can be minimal but never zero).
With NZDB, there is no PLL inside; it is just a Fan-Out buffer. This is not going to filter any jitter at the input and has a propagation delay.
So while making a choice, between in a ZDB and NZDB,
You select a ZDB if your source has a bad jitter that needs filtering and you require a Zero Delay between input and Output. You will also get variants with divider options to have frequency multiplications and divisions and also can adjust skew with ZDBs.
You select a NZDB, if you have a very clean source and need just fanout of the source with less additive jitter. However, your application should be fine with the propagation delay, the NZDB will have. You will have different options to match different signaling standards here.
Show LessAVCMOS name/design came in from one of the companies Cypress acquired, IMI. It is another name for variable output impedance (VOI), or sometimes called variable slew rate (VSR). It is a type of output buffer that has a strong drive current from the beginning of a switch (ie. rise or fall time) to about the mid-point of the switch. At about mid-point, some of the legs of the transistors shut off so that the drive current is reduced, and the resulting transition from mid-point of the switch to the final settling value is smooth (i.e. little overshoot/undershoot). This way, higher frequencies can be achieved without as much overshoot/undershoot. It's called "variable impedance" because the impedance changed depending on whether you're looking at the start of the rise/fall time or the end. Actually, "variable slew rate" is perhaps a more accurate description.
Check the KnowledgeBase Article Titled: AVCMOS Outputs of CY2CC810 Explained at: http://www.cypress.com/?id=4&rID=39987
Show LessThe output impedance of Cypress Zero Delay Buffers is between 20-30 ohm, unless otherwise specified in the datasheets. So its recommended to use a 20-30 ohm series resistor to match a 50 ohm transmission line. Since the output impedance for the ZDBs is between 20-30 ohm, it is recommended to start with (X-28) Ohms series termination placed as close as possible to each output pin (where X is the transmission line impedance you connect to), thus assuming a 28 Ohms output impedance initially. So if you connect the output to 50 Ohms, then 50-28=22 Ohms series termination will be required for impedance matching.
Show Less