Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Clocks Forum Discussions

Sort by:
YTsujio
Clocks
CY27410FLTXI
Solved
We are considering using CY27410 with the following specifications.In the case of the following specifications, can it be realized by using one CY2741... Show More
dalton
Clocks
CY26049
Solved
Hi All, I am using the CY26049-20 as a synchronized clock filtering circuit with  with fall back So I hope to apply a 25MHz ICLK   and obtain a  100 M... Show More
anonymous-sj
Clocks
I just programmed CY29421FLXI-ND using the clockwizard. When look at each output (single ended) on the scope, i see both clk+ and clk- in sync. Basica... Show More
anonymous-sj
Clocks
Does CY29421FLXI-ND support VCXO function? i notice it lacks VC pin. Do I need to disabled this function in clockwizard tool for CY29421FLXI-ND?     Show More
JB_O
Clocks
Hi all, What are the conditions required by Infineon in term of MOQ for having a factory configured CY2545QI ? Also, what would be the extra lead time... Show More
anonymous-sj
Clocks
I am planning to use CY29421FLXI-ND on 3.3V rail, but looks like I2C port is only spec at 2.5V max. is this correct? Can i pull up I2C signals to 3.3V... Show More
anonymous-sj
Clocks
I need help on how to generate programming file for CY29421FLXI-ND to give to the programming house. we need to set the following options: Output=156... Show More
TeMa_2997106
Clocks
I am using CY2305 with the configuration shown in the schematic below. I measured the waveform of CLK1. It has a lot of jitter. (Approximately 2ns) ... Show More
collstep
Clocks
Hi, We use CY2305SXI-1H on a design where we are receiving back for several customer defect reports during start-up at low temperature (lower than 10°... Show More
MAO
Clocks
CSD
Solved

What is the min / max value of Vref of CSDv2?

Forum Information

Clocks

Discussion Forum regarding Clocks topics.