Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Clocks Forum Discussions

Enghofer
Clocks

Hello,

in our design we are using the obsolete CY7B992-7JI. Is a replacement available?

chi3769
Clocks
我們使用了 CY51x7 IC,我們嘗試將低頻晶振設置為 LFF 模式。 我們要使用 50MHz 的晶振,我們按照 LFF 晶振的振盪器相關參數設置。 我們設置振盪器相關參數和 XT-Pattern。但 我們發現如果我們使用 XO_DOUBLER_ENB =1(禁用),我們可以獲得 50MHz 輸出... Show More
TeMa_2997106
Clocks
How should I calculate the power consumption? Is there a spreadsheet that can be calculated? The data sheet have IDDs. However, the number of descript... Show More
TeMa_2997106
Clocks
What is the output impedance of CY27410? In the "Test and Measurement Circuits" of the data sheet, the test environment is described as 50 ohms for si... Show More
beckham
Clocks
We used the CY2071AF as the PLL in our project, as the datasheet mentioned it should be programmable(EPROM) in the field, but we keep failing in the o... Show More
machotico
Clocks
Hello , Please provide the Reliability (JEDEC) and FIT data of the following devices (CYPRESS SEMICONDUCTOR): CY25811SXIT, CY25811SXCT Regards; Luis   Show More
GrCa_1363456
Clocks
Why might the output be inverted? A board using CY2308SXI-1 seems to be inverting the output on bypass mode (S2=1; S1 =0). But according to the data s... Show More
diapulserx
Clocks
Hello, The Cypress CY22801 is listed on the Infineon website as an "active and preferred" device, and I would like to design a product using it.  The ... Show More
Mitchell_shen
Clocks
Have SPEC. define of power noise requirement for design following?  Like Ripple or PSRR number? What is IC internal circuit to rejection power noise? Show More
Flance_Fang
Clocks
Hi. Infineon in the website(Infineon Technologies😞 I can't downloard the clockwizard2.1 install software. whether have you newly clock software, we u... Show More
Forum Information

Clocks

Discussion Forum regarding Clocks topics.