Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Clocks Forum Discussions

Anonymous
Clocks
The default settings for a blank Field programmable device shipped by the factory are all bits set to 0, all outputs tristated, and the crystal oscill... Show More
Anonymous
Clocks
If you configure a programmable device with 0 PPM error and your reference configured has some ppm error to the input frequency, the error at the inpu... Show More
Anonymous
Clocks
Many of you may think of going beyond the datasheet maximum specification of Capacitive Loading.          Generally it is possible to drive two loads ... Show More
Anonymous
Clocks
During power up, important events takes place where the start up registers are loaded to put the part in a start-up condition. If the power ramp is no... Show More
Anonymous
Clocks
There are internal weak pull-down for all the outputs. You do not need to provide pull-downs, however if you would like to provide pull downs, 5K or 1... Show More
Anonymous
Clocks
Any unused outputs should not be connected to anything for non-PLL based buffers like CY2304NZ (NZDB), CY2CC910, CY2DL1510 (HPB) for example. For the ... Show More
Anonymous
Clocks
 AN69091 discusses the Edge Align feature in Cypress’s programmable clock family, CY254xx and MoBL® clocks. Today’s technology products operate at GHz... Show More
Anonymous
Clocks
FleXO™ is a family of low phase noise clock generators and oscillators, consisting of both fixed frequency devices and programmable devices and with p... Show More
Anonymous
Clocks
 Have a look at this video and application note for Understanding  of Zero Delay Buffers and its different Applications.    http://www.cypress.com/?rID=12622... Show More
Anonymous
Clocks
High Performance Buffers CY2DP1502, CY2DP1504 and CY2DP1510 now support HCSL as well at the inputs. Accordingly, Cypress updated respective datasheets... Show More
Forum Information

Clocks

Discussion Forum regarding Clocks topics.