Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Clocks Forum Discussions

Anonymous
Not applicable

Hello All,

   

Im using CY8C4127LQI-BL473 for my application. What is the maximum clock frequency that i can generate from 'Clock' resource in psoc creator? I need it to generate a sine wave using PWM and filtering. For e.g., Im trying to get 500kHz PWM with 24MHz clock which gets me period count of 48. If i can increase the input clock the resolution can increase as well?

   

Thanks

   

Ashutosh

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Max frequency for your selected chip is 24MHz. When you use a CY8C4247LQI-BL473 you may use 48MHz for sysclk.

   

 

   

Bob

View solution in original post

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Max frequency for your selected chip is 24MHz. When you use a CY8C4247LQI-BL473 you may use 48MHz for sysclk.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thanks Bob. 🙂

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

You are always welcome, Ashutosh.

   

 

   

Bob

0 Likes