Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello everybody,

   

maybe I'm only blind, but I can not figure out how to enable the VCXO,OE and PD features on the CY22801 in CyClocksRT...

   

I'd like to use either the CY22800 or CY22801 chip to generate a 55,5MHz clock from a 10MHz crystal + VCXO.

   

10MHz -> 55,5MHz on the CY22800 is not possible with InstaClock, as I can only use the predefined configurations.
Or is there a similar feature to select multiplicator/divider settings as is in CyClicksRT for the CY22801?

   

On the other hand, I can specify 10MHz -> 55,5MHz on the CY22801 with CyClocks, but I can not see how to enable the VCXO.

   

Best regards
Andreas

0 Likes
0 Replies