- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all,
I'm writing an IIO driver in C for the Cypress CY22801, with communications via I2C.
However, setting the two available output clock channels generically will be difficult, as there are a lot of variables involved.
For example, I will have to calculate the values for PB, PO, Q, and DIVxN, and select the most suitable divider channel (1/2), and set the source controls for the clock outputs, for each clock output - each will affect the other one, also.
i.e. CLK_OUT_X = (2 * (pb + 4) + po) / (q + 2) / DIVxN * CLK_INPUT_FREQ
The CyClocksRT software generates all of this information automatically. Is the source code for this component of the software available, please? Or can a version of this be provided to aid our use of your products?
Many thanks,
Adam
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @AdamWilsonCPI ,
Unfortunately, we can not provide the source code as it is the company confidential thing.
Apologies for the inconvenience.
Thanks and Regards,
Nitin
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
Hi Nitin,
I already have the latest software installed, thank you.
I was wondering whether the source code is available for it, or at least a snippet for where all of the register configuration is done based on the selected output frequencies?
Many thanks,
Adam
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
Hi Nitin,
I have the register map from the datasheet, thank you.
I want to configure this part dynamically at runtime via I2C. It should be possible to set an output setpoint frequency for CLKA and CLKC via SysFS on Linux, and the IIO driver I'm building should be able to setup the CY22801 as required.
This requires calculating the required values for all of the control registers based on the selected output clock frequencies, which is what the CyClocks software does to create a JDEC file.
If I had access to the related parts of the CyClocks source code, I would be able to do the same, but at runtime.
I could manually create a look-up table based on manually-generated output files from CyClocks, but this would take a long time, and the look-up table would be huge.
Many thanks,
Adam
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @AdamWilsonCPI ,
Unfortunately, we can not provide the source code as it is the company confidential thing.
Apologies for the inconvenience.
Thanks and Regards,
Nitin