Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NoAr_1540581
Level 5
Level 5
Distributor - Macnica (Japan)
5 solutions authored 250 sign-ins 100 replies posted

Hello

Q)

If CLKA3(14pin)  is not used, please tell me pin proccessing of unused pin(CLKA3) as an "EMI" countrmeasure? Is CLKA3(14pin) open? Or is it necessary to add the capacitor? (Other port condition): CLKB1, CLKB2, CLKB3, and CLKB4 are not driven.

In addition, they found the following application note ,it is described that If EMI is a problem, mount a 5pF to 10pF capacitor during testing on page 6.

>https://www.cypress.com/file/194861/download

Best Regards

Arai

0 Likes
1 Solution
ShupingZ_76
Employee
Employee
50 solutions authored 25 solutions authored 10 solutions authored

Hi Arai-san,

Typically, the unused output pins are left open.

If the EMI countermeasure for the output pin is desired, a capacitor could be attached.

This method will reduce EMI for higher frequency, but it will also increase the power consumption.

Best regards,

Shuping

View solution in original post

0 Likes
1 Reply
ShupingZ_76
Employee
Employee
50 solutions authored 25 solutions authored 10 solutions authored

Hi Arai-san,

Typically, the unused output pins are left open.

If the EMI countermeasure for the output pin is desired, a capacitor could be attached.

This method will reduce EMI for higher frequency, but it will also increase the power consumption.

Best regards,

Shuping

0 Likes