Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Class D Audio Amplifier IC Forum Discussions

Sort by:
KRummery
Class D Audio Amplifier IC
Hello, I am using a MA12040P for audio playback of a I2S stream being produced by the SAI peripheral of an iMX8M Plus. I have ported the driver from t... Show More
PhilGood_82
Class D Audio Amplifier IC
Hi  With IRS2452AM, application notes and examples describe 400kHz switching frequency (IRAUDAMP23 for exemple). How modify values to get self-oscilla... Show More
PhilGood_82
Class D Audio Amplifier IC
Hello everybody Using IRS2452AM for class D amplifier solution, we face a problem when output current on the load increases : output signal is disrupt... Show More
Artur
Class D Audio Amplifier IC
Hello, I wander if chip name MA5332M is real product of Infieon. Is this the same as MA5332MS? Chip MA5332M is inside Sabaj amplifier, is it real Infi... Show More
Julian66
Class D Audio Amplifier IC
Hi Sirs, I have a MA2304DNS EVAL Board, I can use this EVK to play music to speaker. But it seems not working when I adjust EQ, here is the procedure:... Show More
Happy
Class D Audio Amplifier IC
笔记本电源19.6V 输入到电路,然后启用设备: /ENABLE = 0.Unmute device: /MUTE = 1.,PBTL模式输出20V直流电,但是如果只输入9v工作正常,请教一下专家原因,PCB检查很多次没有问题。 Show More
Ravi
Class D Audio Amplifier IC
Hello, Kindly help me with the following questions: 1. What should be the preferred voltage on MSEL0, MSEL1, nMUTE, nENABLE, nClip, nERROR, SCL, SDA, ... Show More
Ravi
Class D Audio Amplifier IC
Hello, I would like to design a PCB for the MA12070 IC. I have following queries. Kindly help me with them. Thanks in advance! 1. Datasheet recommends... Show More
Katie1
Class D Audio Amplifier IC

I am trying to find out what the 1 stands for in the PN: MA12070P1 and if this part can be used instead of MA12070P ?

Michaellu
Class D Audio Amplifier IC
 i want to evaluate ic ma2304 and make a ma2304 demo board. i have two issues。 1.Is the schematic correct in User manual for MA evaluation boardsMA230... Show More
Forum Information

Class D Audio Amplifier IC

In this forum you can post your questions, comments and feedback about the Infineon Merus range of mid power and high power Class D Amplifiers that range from 10Watts to 5kW! Infineon’s Merus Audio amplifiers range from Analog Input Discrete Class D amplifiers for Home, Professional and Aftermarket Automotive amplifiers through to highly integrated digital I2S input Class D amplifiers for portable and home active speakers. Post your questions below to get feedback from our team of audio experts. For the quickest response please share parts of your schematic, layout and configuration data. Below you’ll also find links to the latest board pages, GitHub, documents and FAQs.