Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Class D Audio Amplifier IC Forum Discussions

Sort by:
Aa1987
Class D Audio Amplifier IC
Dear Developer team / community, I'm looking for a diagram of the Class D amplifier as the attached photo, is it possible? Thanks so much!   Show More
Wineopener
Class D Audio Amplifier IC
Piezo driver
solved msg Solved
HI, Do you have Piezo driver devices  for buzzer or speaker? Or,  Can you make  solutions of  Class-D amps for Piezo ?  Best Regards, BANE Show More
GabeLongo
Class D Audio Amplifier IC
I'm using the EVAL_AUDIO_MA2304DNS at 192kHz fs. Currently I have 2 channels that each have 2 biquads configured to be filters. In total I'm using 4 o... Show More
GabeLongo
Class D Audio Amplifier IC
I have an EVAL_AUDIO_MA2304DNS, it's connected to the GUI and I'm trying to apply a cross over filter to an incoming signal with the integrated DSP. I... Show More
Przemek6
Class D Audio Amplifier IC
Hello, I have a question regarding MA2304 and power supply. According to user manual (v 1.1) pin no. 40 can be connected to PVDD or VDD (J_VDD). If we... Show More
yogeshks1
Class D Audio Amplifier IC
Dear Team we are aiming to develop a class D amplifier 2CH and 4 CH . Our present design is based on IRS2092, for 500w system new amp is target to del... Show More
The_BOOM
Class D Audio Amplifier IC
Can any Class-D chip  be used as a power supply?   The idea is to use the same topology as a Class D amplifier, but the following specs: AC constant... Show More
yogeshks1
Class D Audio Amplifier IC
Dear Team this is regarding the IRS 2452 chip, used to make constant voltage distribution system, IRAUDAMP 23 is reference design for  500 W x 2 chan... Show More
Fini
Class D Audio Amplifier IC
Dear Infineon community, I get a pop noise every time I mute or unmute the amp, even when I keep the amp enabled, I2S clock continuously on and with d... Show More
Diegoalm
Class D Audio Amplifier IC
I have two MA12070 chinese boards and neither of them sounds when I connect them no matter how they don't sound, I realized that the enable PIN was se... Show More
Forum Information

Class D Audio Amplifier IC

In this forum you can post your questions, comments and feedback about the Infineon Merus range of mid power and high power Class D Amplifiers that range from 10Watts to 5kW! Infineon’s Merus Audio amplifiers range from Analog Input Discrete Class D amplifiers for Home, Professional and Aftermarket Automotive amplifiers through to highly integrated digital I2S input Class D amplifiers for portable and home active speakers. Post your questions below to get feedback from our team of audio experts. For the quickest response please share parts of your schematic, layout and configuration data. Below you’ll also find links to the latest board pages, GitHub, documents and FAQs.