Announcements

Join us for FREE at OktoberTech Asia Pacific and hear about decarbonizing future mobility. Click here for more details.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Class D Audio Amplifier IC Forum Discussions

User18221
Level 1
First question asked
Level 1
Hello Sir,

My intention is to make an 3-phase power calibrator, https://us.flukecal.com/products/ele...wer-calibrator
I was looking for a ClassD solution, https://e2e.ti.com/support/audio/f/6/t/842164

Many people says " potential transformer PT can be applicable with TPA3220(analog input), or TAS5760M or TPA3116D2". Mostly they are , Speaker Bar, Docks or Consumer Audio Application.
My case is different.

My requirements were,
REQUIRMENTS :
1. The amp input should be plus and minus 7volt AC, 45-65Hz( 1 Hz has been converted to 1024)
2. Amp operating voltage should be more or less 24v.
3. 2 channel signal (not sure PWM) should be use , one for current, one for voltage.
4.Can run current transformer(input 16.5 V/1.5 A) and potential Transformer (input15v/2A). PT output may be 15VAC.
5. If possible both voltage and current amplification is required in one IC.
6. Both positive and negative half signal should be amplify. ( take a look bellow For CT, current transformer primary winding has 80turns, 16.5 V/1.5 A, secondary has 20Turns, 4.125v/6A output! For PT, Potential transformer, Primary has 80turns, 15v/2A rating input, secondary has centertap! At secondary 960turns, 360v/0.332 A and 960turns 180v/0.166A output.

I wanna move to Bridge type/SMPS type application, since it looks little bit high current and voltage application.

Most probably the challenge is to control facilities, since my system has instruction from central stm32!


Any infineon product is appreciable !






HW Engineer
Hasan
0 Likes
1 Solution
PranavaYN
Moderator
Moderator 50 likes received First comment on KBA First question asked
Moderator

Hi,

You can use one of our Class D Audio Amplifier solution for voltage amplification based on power rating - https://www.infineon.com/cms/en/product/power/class-d-audio-amplifier-ic/?gclid=Cj0KCQjw6pOTBhCTARIs...  It is not possible to connect this output to a Current transformer.

You can explore our range of DC-DC Converters for current amplification - https://www.infineon.com/cms/en/product/power/dc-dc-converters/

 

 

Best regards,
Pranava

View solution in original post

1 Reply
PranavaYN
Moderator
Moderator 50 likes received First comment on KBA First question asked
Moderator

Hi,

You can use one of our Class D Audio Amplifier solution for voltage amplification based on power rating - https://www.infineon.com/cms/en/product/power/class-d-audio-amplifier-ic/?gclid=Cj0KCQjw6pOTBhCTARIs...  It is not possible to connect this output to a Current transformer.

You can explore our range of DC-DC Converters for current amplification - https://www.infineon.com/cms/en/product/power/dc-dc-converters/

 

 

Best regards,
Pranava