CAPSENSE™ & MagSense Forum Discussions
Hi, Infineon team,
I want to know how to design for CSX Touchpad.
It seems that there is the document of AN234185 PSoC™ 4 CAPSENSE™ Touchpad design guide .
But I can't reach this link: https://www.infineon.com/002-34185
The PCB reference data has been gotten from the link in this thread.
https://community.infineon.com/t5/ModusToolbox/PSOC-capsense-touchpad-handwriting/m-p/381127#M497
However, I would like to know the design rules, and why these designs should be used.
If possible, could you provide me the AN234185?
Best Regards,
Show LessHello,
When two different types of overlays are stacked.
What is the formula for calculating capacitance?
In the case of one overlay, the following is
When overlaying two different types of overlays,
(The following is an image. For example, OVERLAY1 is glass, OVERLAY2 is PET film)
What is the formula for calculating capacitance?
(For example, will overlay 2 be added?)
Best Regards,
Kawata
你好,关于MBR3设置了自动阈值调整,请问下阈值根据哪个参数,以怎么样的形式进行调整的?以什么的标准进行调整?在界面上可设置的参数太少,无法判定阈值是否可靠?因为观察到用同一铜柱进行测试,Rawdata变化基本不变,但是SNR确是随着触摸,逐渐减小,为什么?SNR计算的标准不是信号量/噪声吗?以上是我的理解,请协助下
Show Less
据我所知,第五代CAPSENSE相比第四代将电容(包括自电容+互电容技术)和电感触摸技术集成到了一起,SNR信噪比是上一代的十多倍,同时功耗仅是上一代的十分之一。但是这张图在感应模式上第四代和第五代似乎别无二致,我想知道是不是第四代CAPSENSE技术只是不能同时支持这三种模式,但是可以不同时支持?
Show Less
Hello,
If the overlay has a slope as shown in the image below,
Is there anything I should be careful about when adjusting CAPSENSE?
(The following is an image)
How should I consider the capacitance when touched?
(Is it just the thickness of the overlay at the touched position?)
Best Regards,
Kawata
Show Less
Is there any information on the frequency attenuation of TLE4973 for CRTF values for different busbar sizes?
For example, in vertical mode, Busbar width is 18mm, thickness is 3mm, other sizes are also available.
What are the CRTF values at DC, AC@1kHz, AC@2kHz, and AC@10kHz?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%B5%81-%E6%AD%A4%E5%9E%8B%E4%BC%A0%E6%84%9F%E5%99%A8/TLE4973-%E5%AF%B9%E5%BA%94%E4%B8%8D%E5%90%8Cbusbar%E5%B0%BA%E5%AF%B8%E7%9A%84CRTF%E5%80%BC%E7%9A%84%E9%A2%91%E7%8E%87%E8%A1%B0%E5%87%8F/td-p/715929
Show LessGood morning everyone, I have a system with Psoc4100S-Plus, VDDA at 5V and VDDD at 3.3V.
The CapSense block is powered by VDDA.
Why is the Tx signal for CSX mode 3.3V?
Can it be set to 5V of VDDA?
What is the process rule of PSoC4000T? Is it same as PSoC4 series(130nm)?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/CAPSENSE%E3%81%8A%E3%82%88%E3%81%B3MagSense/process-rule-of-PSoC4000T/td-p/716247
Show LessHi,
I was was researching input methods/switches for desktop use and I stumbled across this device https://www.native-instruments.com/en/products/maschine/production-systems/maschine-plus/ . I was able to interact with this device and what caught my interest the most were the (presumably) capacitive pads (the 4x4 grid with big rectangular buttons). They felt super responsive and I wanted to try and make a keyboard using similar type of input. I am confused, however, as to what components I would need for that project. The ones i'm unsure about are the buttons (I had a look at the MBR3 evaluation kit but I can't tell how the buttons are construted) that would sit behind the block of plastic (or other appropriate material similar to the one on the maschine device - I do want these to protrude out similar to keys on a keyboard), the touch microcontrollers, and then microcontrollers that are collecting the output from these. Eventually I want to go up to a tkl design which uses 108 keys. I also care about latency and reliability so a 1kHz polling would be expected (although I would consider designs up to 10kHz).
I am completely green when it comes to pcb design so I'd appreciate any help
Show Less