CAPSENSE™ & MagSense Forum Discussions
Hello,
PSoC Creator component datasheet (PSoC4 CapSense) have been updated from v7.0 to 7.0a, 7.0b and 7.1.
However I can't find any difference in the Generated library code(.c and .h) and binary(.hex).
What is the difference between version 7.0 and 7.1?
Are there any functional differences?
MPN CY8C4025LQI-S411
Best Regards,
Naoaki Morimoto
Show LessHello Infineon.
Below link has a description of the Layout rule checklist(Table 41).
But there is no mention of proximity.
Is there a checklist of layout rules regarding proximity sensors?
Also, is it possible to use a curved overlay?
Or is only a flat overlay recommended?
Best Regards.
YuMa
Show LessHello.
I have a PGSISI board for linear Hall sensor.
I got Angle IC (TLE5014C), I assume I could use same board, nut coule it be possible to get the GUI SW for windows?
Thank you.
Show LessHello,
I want to use tuner helper for CY8C4245AXI-483 for touch switch. Is sample code for using tuner helper available for this particular controller?
The reason for asking for code is that I have made a few changes in design. Is it necessary to measure signal (raw count - baseline) for setting proper value of finger threshold or it can be done on trial and error basis.
I have FT value of 85 and it's working fine, but want to check for new design changes.
Please let me know if FT must be set after calculating signal (80 % of signal) or can I skip using tuner helper and set FT manually?
Thank you.
Are the measurement range for angular measurement of TLE4999C4 and TLE4998S chipsets 0 to 360 degrees?
Not sure if this is the best spot for this. Trying to create a demo application for the PSoC4 4100S Max Pioneer Kit using ModusToolbox. Specifically, the demo CSD touchpad app. When it goes to build the app, I get a bunch of error messages:
Failed to commit changes to the project 'mtb-example-psoc4-msc-capsense-csd-touchpad-tuning'.
Failed to process project 'MSC_CAPSENSE_CSD_Touchpad_Tuning_1'.
Application creation failed.
This gets followed by a bunch of red text with more error messages.
I've tried twice now. Any ideas what I'm doing wrong?
Show LessHi team,
I am using IC CY8CMBR3108 to make touch switch. I am trying to config IC base on document about register. And I am having a problem about CONFIG_CRC register.
1. As I know, I need to calculate checksum all value of register (CRC 16) and write in this register and save it. I understand that right? How can I calculate it?
2. Can I configure a single register? How to calculate checksum in this case?
Thank for your help.
Quoc Anh.
Show Less
Does anyone know how to use the touch chip CY8CMBR3108? I currently want to implement both click and slide functions, should the chip pin be connected directly to the touch point or connected through a series resistor, can my sliding part be connected to the touch function after using a sawtooth arrangement?I read the datasheet for several times but I cannot sure the usage of this chip.
Hi there,