CAPSENSE™ & MagSense Forum Discussions
Hi,
I want to design a capacitive touch application with a brass metal plate. So, i need a sensor that is suitable with brass metal. Is there any advised product for me?
Thanks
Show LessHello Infineon.
Is there a graph that shows the relationship between sensor pattern length and proximity detection distance?
Our customer wants to know how the proximity detection distance changes when the length of the sensor pattern changes.
I found the graph below from the Infineon documentation.
Is there any data that shows the relationship between sensor pattern length and proximity detection distance other than this?
If possible, I would like to have data without ALP conditions.
I understand that ALP does not support 4th and 5th generation CapSense, is that correct?
Target device is 5th generation CapSense.
Best Regards.
YuMa
Show LessHello,
PSoC Creator component datasheet (PSoC4 CapSense) have been updated from v7.0 to 7.0a, 7.0b and 7.1.
However I can't find any difference in the Generated library code(.c and .h) and binary(.hex).
What is the difference between version 7.0 and 7.1?
Are there any functional differences?
MPN CY8C4025LQI-S411
Best Regards,
Naoaki Morimoto
Show LessHello Infineon.
Below link has a description of the Layout rule checklist(Table 41).
But there is no mention of proximity.
Is there a checklist of layout rules regarding proximity sensors?
Also, is it possible to use a curved overlay?
Or is only a flat overlay recommended?
Best Regards.
YuMa
Show LessHello.
I have a PGSISI board for linear Hall sensor.
I got Angle IC (TLE5014C), I assume I could use same board, nut coule it be possible to get the GUI SW for windows?
Thank you.
Show LessHello,
I want to use tuner helper for CY8C4245AXI-483 for touch switch. Is sample code for using tuner helper available for this particular controller?
The reason for asking for code is that I have made a few changes in design. Is it necessary to measure signal (raw count - baseline) for setting proper value of finger threshold or it can be done on trial and error basis.
I have FT value of 85 and it's working fine, but want to check for new design changes.
Please let me know if FT must be set after calculating signal (80 % of signal) or can I skip using tuner helper and set FT manually?
Thank you.
Are the measurement range for angular measurement of TLE4999C4 and TLE4998S chipsets 0 to 360 degrees?
Not sure if this is the best spot for this. Trying to create a demo application for the PSoC4 4100S Max Pioneer Kit using ModusToolbox. Specifically, the demo CSD touchpad app. When it goes to build the app, I get a bunch of error messages:
Failed to commit changes to the project 'mtb-example-psoc4-msc-capsense-csd-touchpad-tuning'.
Failed to process project 'MSC_CAPSENSE_CSD_Touchpad_Tuning_1'.
Application creation failed.
This gets followed by a bunch of red text with more error messages.
I've tried twice now. Any ideas what I'm doing wrong?
Show LessHi team,
I am using IC CY8CMBR3108 to make touch switch. I am trying to config IC base on document about register. And I am having a problem about CONFIG_CRC register.
1. As I know, I need to calculate checksum all value of register (CRC 16) and write in this register and save it. I understand that right? How can I calculate it?
2. Can I configure a single register? How to calculate checksum in this case?
Thank for your help.
Quoc Anh.
Show Less
Does anyone know how to use the touch chip CY8CMBR3108? I currently want to implement both click and slide functions, should the chip pin be connected directly to the touch point or connected through a series resistor, can my sliding part be connected to the touch function after using a sawtooth arrangement?I read the datasheet for several times but I cannot sure the usage of this chip.