CAPSENSE™ & MagSense Forum Discussions
Hello,
If the overlay has a slope as shown in the image below,
Is there anything I should be careful about when adjusting CAPSENSE?
(The following is an image)
How should I consider the capacitance when touched?
(Is it just the thickness of the overlay at the touched position?)
Best Regards,
Kawata
Show Less
Hi Community,
I am getting issues in reading tuner data. It is not getting connected. I need help to debug this issue.
Regards D
L9663 PSI5 convert SPI protocol chip, there are no routines, the supplier did not ask for it!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/CAPSENSE-MagSense/L9663-%E4%BE%8B%E7%A8%8B/td-p/717848
Show LessIs there any information on the frequency attenuation of TLE4973 for CRTF values for different busbar sizes?
For example, in vertical mode, Busbar width is 18mm, thickness is 3mm, other sizes are also available.
What are the CRTF values at DC, AC@1kHz, AC@2kHz, and AC@10kHz?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E7%94%B5%E6%B5%81-%E6%AD%A4%E5%9E%8B%E4%BC%A0%E6%84%9F%E5%99%A8/TLE4973-%E5%AF%B9%E5%BA%94%E4%B8%8D%E5%90%8Cbusbar%E5%B0%BA%E5%AF%B8%E7%9A%84CRTF%E5%80%BC%E7%9A%84%E9%A2%91%E7%8E%87%E8%A1%B0%E5%87%8F/td-p/715929
Show LessGood morning everyone, I have a system with Psoc4100S-Plus, VDDA at 5V and VDDD at 3.3V.
The CapSense block is powered by VDDA.
Why is the Tx signal for CSX mode 3.3V?
Can it be set to 5V of VDDA?
What is the process rule of PSoC4000T? Is it same as PSoC4 series(130nm)?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/CAPSENSE%E3%81%8A%E3%82%88%E3%81%B3MagSense/process-rule-of-PSoC4000T/td-p/716247
Show LessHi,
I was was researching input methods/switches for desktop use and I stumbled across this device https://www.native-instruments.com/en/products/maschine/production-systems/maschine-plus/ . I was able to interact with this device and what caught my interest the most were the (presumably) capacitive pads (the 4x4 grid with big rectangular buttons). They felt super responsive and I wanted to try and make a keyboard using similar type of input. I am confused, however, as to what components I would need for that project. The ones i'm unsure about are the buttons (I had a look at the MBR3 evaluation kit but I can't tell how the buttons are construted) that would sit behind the block of plastic (or other appropriate material similar to the one on the maschine device - I do want these to protrude out similar to keys on a keyboard), the touch microcontrollers, and then microcontrollers that are collecting the output from these. Eventually I want to go up to a tkl design which uses 108 keys. I also care about latency and reliability so a 1kHz polling would be expected (although I would consider designs up to 10kHz).
I am completely green when it comes to pcb design so I'd appreciate any help
Show LessWe have experience tuning PSoC1 and PSoC4 non-MAX ICs to sense through thick gloves or even 5mm+ of cover glass. However, we are still learning about the CapSENSE 5 capabilities found in the PSoC4 MAX. Using the Pioneer kit, I've been able to overlay about 4mm of cover glass on the touchpad found on the expansion board and still get good response, but haven't experimented further. Has anyone out there explored the limits of what's possible for sensing distance using the PSoC4 MAX? Anyone hit 10mm? Obviously, this will be dependent on sensor design/construction.
Show Less