Recent discussions
Hi Infineon Team,
I am using cy8mbr3108 capsense. I am using linux platform and using i2cdetect utility for detecting the touch sensor over I2C. I found that sometime it is able to detect the sensor and sometimes not. If I detect it too fast, then it is able to detect, otherwise not. I learned from datasheet that it is in deep sleep mode by default. It sends NACK before going it to ACTIVE state. So, need to perform address match again!! Any way of moving device out of deep sleep mode? How to avoid polling?
Another secondary question is , lets say the device is detected once and then going to write I2C register, at that time it might not be able to write as it will be in deep sleep right?
Regards,
Kunal
Show LessHello,
I need some help how to start tuning with CY8CKIT-149 kit. I need to get demo working to put slider and buttons to glass overlay of 2mm thickness.
- Should i start with Auto-tuning or manual tuning? could you recommended documentation how to do tuning?
- Slider is placed to glass surface. Should i remove Acrylic overlay from slider(from dev kit)?
Best regards
Teijo
Show LessI want to tune the CapSense sensors, So for software parameters are there any prescribed values from where we need to start tuning or We have to select tuning parameters randomly(in a hit and trial manner) and then we have to further change those parameters to get the best result? Basically, How to start the tuning process of the sensor. Also please share some document to know the details about these paramters and what they signify?
Thanks
Show LessHi,
I wanted to make a sample project of CapSense and I got to know that we have to take care of the parasitic Capacitance value. I wanted to calculate the parasitic capacitance value of the sensor and I am using GetSensorCapacitance() function to print the value but PSoC creator is throwing undefined reference to GetSensorCapacitance error in PSoC Creator. Can you tell why it is happening? How to solve the error? Also, Is there a range of Parasitic Capacitance upto which CapSense can support?
Regards D
Show Lessお世話になっております。
Capsenseのdesign guideのManually tuning hardware parameters、Sense clock frequencyに下記記載がございます。
Equation 25 shows that it is best to use the maximum clock frequency to have a good gain; however, you
should ensure that the sensor capacitor fully charges and discharges as shown in Figure 39.
このthe sensor capacitor fully charges and dischargesはどのように確認を行えばよろしいでしょうか?
ご教示いただきたく、よろしくお願いいたします。
Show Lessいつもお世話になっております。
Capsense_Configration.hの下記変数の値の変化要因は何になるでしょうか?
・CapSense_CSD_GAIN
・Capsense_ADC_GAIN
・Capsense_ADC_IDAC_DEFAULT
なお、顧客プロジェクト(ICはCY8C4024LQI-S411)上では主だったところで
・Sense clock frequency
・Finger Threshold
・VDD(Design wide Resourceのsystem上)
を変えたところ、上記の3変数(およびCapSense_CSD_VREF_MV、Capsense_ADC_VREF_MV)が変わっているとの事です。
以上、ご教示いただきたく、よろしくお願いいたします。
Show Lessit seems like I'll be getting an Infineon based TSDZ2.
Has anyone managed to use a J-Link to flash/program/configure the stock firmware to support 52V?
If so, how? Are there any resources I'm not aware of? I can't seem to find anything.
Any insight is massively appreciated.
Show LessHello,
I want to use a PSoC 4 device to continuously measure the raw capacitance of a two terminal capacitive sensor. The examples I found seem to detect changes in capacitance beyond a certain threshold, rather than measuring and outputting the raw capacitance value across two terminals. How would I do this? Are there any examples to follow?
Thanks!
Show LessWho can I contact to get Cypress CapSense support?
None of the original links in the datasheets seem work and I can't find the information to get started.
Also, where is the roadmap?
Eval boards?
Application notes?
We are Australia based.
Regards
B
Show Less
Hi all,
We are planning to use CY8CMBR3108 Capsense for our Linux product. I came to know that we can do the configurations from the modus tool. However, for communication with application I would need to have Linux driver which will communicate with Capsense and fetch the data. This driver then provide the data to user application. I looked into it , but I didn't found any Linux driver support. Can anyone help me with whether we have such linux driver for Capsense or not?
Regards,
Kunal
Show Less