Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

kuon
Level 1
Level 1
5 sign-ins First reply posted First question asked

Hello,

I am designing a product for medical liquid sensing and I am a bit lost in all your products.

My tank is about 20cm high, and I need a 1mm accuracy (so 200 divisions). My sensor PCB can be up to 3cm wide (so 20cm x 3cm for sensor).

The distance between the liquid and the PCB is 2.5mm PVC, 0.5-1mm air, and 1.5mm ABS.

I was wondering if you had recommendation on which product to use, and how many (segmentation of the sensors). I already have a microprocessor in my product and only need the sensing part (via like I2C).

1 Solution
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi @kuon

 

In both cases, I would recommend our PSoC 4S line of devices - PSoC 4000S, PSoC 4100S and PSoC 4100S plus. 

You can evaluate the performance using the kits:
CY8CKIT145-40XX - PSoC 4000S

CY8CKIT-041-41XX - PSoC 4100S

CY8CKIT-149 - PSoC 4100 S Plus

 

PSoC 4100S Plus is the most advanced CapSense IP with a higher GPIO count as well. 

 

Best regards, 
Hari

View solution in original post

0 Likes
8 Replies
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi @kuon

 

Can you please provide additional details before we suggest a sensing method?

1. Is the liquid being sensed conductive or non-conductive? Is there any possibility of the liquid being grounded? (Note that the sensing method is dependent on the type of liquid). 

2. If the liquid is conductive and grounded, can it be ensured that it is always connected to the ground and its not an accidental ground connection? If its not grounded, can it be ensured that there is no possibility of accidental grounding?

3. What is the dimension of the inner part of the container where the liquid will be present? And what is the volume of the container?

4. Is the air gap provided for thermal isolation? Can this be avoided for improvements in liquid level sensing? 

 

Best regards, 

Hari

0 Likes
kuon
Level 1
Level 1
5 sign-ins First reply posted First question asked

The liquid a composition of different body fluid that can vary in conductivity from 1 to 50 mS. It is not grounded and there is a drip chamber so accidental grounding should not happen and the device is battery operated.

The dimension of the inner part of the container is about 5cm x 15cm x 18cm, but we plan wider container with the middle dimension being bigger. The volume will be from 1.2l to 2.5l with the 5cm (depth) and 18cm (height) not varying. So there is about 5cm of liquid in front of the sensor.

 

The air gap is variable play gap, the container is a single use consumable and it is mounted on another part containing the sensor, when mounted, there is a small possible air gap as the flatness of the consumable container is not 100% guaranteed because of production constraints.

0 Likes
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi @kuon

 

Obtaining an accuracy of 1 mm would not be possible with the current configuration. The main issue is the variable air gap formed between the disposable container and the main container. Would it be possible to mechanically change the design to avoid this?


If it is not possible, can the accuracy be close to 5 mm? 

 

Best regards, 
Hari

0 Likes
kuon
Level 1
Level 1
5 sign-ins First reply posted First question asked

Can you tell me what you would recommend if I can get rid of the air gap, and what you recommend if I cannot (with 5mm accuracy)? I will then experiment with it and see what I get.

0 Likes
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi @kuon

 

In both cases, I would recommend our PSoC 4S line of devices - PSoC 4000S, PSoC 4100S and PSoC 4100S plus. 

You can evaluate the performance using the kits:
CY8CKIT145-40XX - PSoC 4000S

CY8CKIT-041-41XX - PSoC 4100S

CY8CKIT-149 - PSoC 4100 S Plus

 

PSoC 4100S Plus is the most advanced CapSense IP with a higher GPIO count as well. 

 

Best regards, 
Hari

0 Likes
kuon
Level 1
Level 1
5 sign-ins First reply posted First question asked

I already have a processor in my design, do you have "dumb" sensor that I can use via I2C or similar?

Also, do you have a design document to design the sensors traces? I plan to use an fr4 PCB, and I wonder what size I should make the sensor pads, and also if I should segment it or not, what shape, etc...

0 Likes
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi @kuon 

 

Our I2C configurable controller, called MBR3, would not be suitable in this application as liquid level sensing requires manual tuning. You can still use the PSoC 4S device as the sensor and communicate the data to your host using any communication protocol of your choice - note that the code must be written for the same. 

 

Coming to sensor design, we have two documents.

1. CapSense design guide, which explains the basics of CapSense sensor design, trace routing, routing with digital signals around etc. This document also has a schematic and layout rule checklist as well (page 128). 

2. For liquid level sensing specifically, you can refer to PSoC® 4 - Capacitive Liquid-Level Sensing where you can check out the sensor patterns  (Section 3.5) and other LLS related parameters. 

 

Please note that we can help you with the design and provide a review once the initial design is ready.

 

Best regards, 
Hari

0 Likes
kuon
Level 1
Level 1
5 sign-ins First reply posted First question asked

Thank you, I will play with your kits and come back if I have any more question.

 

0 Likes