- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I would like to make buttons that can detect a conductive object put on the overlay.
I was thinking about using the CY8CMBR3110 and self capacitance measurement but I don't know what configuration would be best as the object won't be connected to ground.
- Configuration 1 : Sensors with a fishbone pattern (Rx = capsense signal and Tx = ground) with hatched ground plane connected to Tx (but won't my parasitic capacitance be too high ?)
- Configuration 2 : Sensors with a fishbone pattern (Rx = capsense signal and Tx = ground) with hatched ground plane but clearance between Tx and ground plane
- Configuration 3 : Round sensors with hatched ground (normal button configuration if you want to detect touch event)
- Or something different ?
Also is it possible to use several buttons at the same time ?
Lastly, if we disabled the auto reset, how long the sensor can stay in the ON position ? Can we let an object on the sensor for several hours and the presence will still be recognized ?
Thanks in advance,
Have a nice day
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @ltdndt
What is the size of the object that needs to be detected? If it is a large object that can extend to the hatched ground region, then Configuration 3, Round sensor can be used as this would induce larger coupling to ground to the conductive object.
Also, how many sensors are planned to be used for object detection?
If the sensor auto-reset is turned off, then the sensor will report the ON status till it is reset (either by XRES or power cycle).
Best regards,
Hari