- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I would like to make buttons that can detect a conductive object put on the overlay.
I was thinking about using the CY8CMBR3110 and self capacitance measurement but I don't know what configuration would be best as the object won't be connected to ground.
- Configuration 1 : Sensors with a fishbone pattern (Rx = capsense signal and Tx = ground) with hatched ground plane connected to Tx (but won't my parasitic capacitance be too high ?)
- Configuration 2 : Sensors with a fishbone pattern (Rx = capsense signal and Tx = ground) with hatched ground plane but clearance between Tx and ground plane
- Configuration 3 : Round sensors with hatched ground (normal button configuration if you want to detect touch event)
- Or something different ?
Also is it possible to use several buttons at the same time ?
Lastly, if we disabled the auto reset, how long the sensor can stay in the ON position ? Can we let an object on the sensor for several hours and the presence will still be recognized ?
Thanks in advance,
Have a nice day
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @ltdndt
What is the size of the object that needs to be detected? If it is a large object that can extend to the hatched ground region, then Configuration 3, Round sensor can be used as this would induce larger coupling to ground to the conductive object.
Also, how many sensors are planned to be used for object detection?
If the sensor auto-reset is turned off, then the sensor will report the ON status till it is reset (either by XRES or power cycle).
Best regards,
Hari
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @ltdndt
What is the size of the object that needs to be detected? If it is a large object that can extend to the hatched ground region, then Configuration 3, Round sensor can be used as this would induce larger coupling to ground to the conductive object.
Also, how many sensors are planned to be used for object detection?
If the sensor auto-reset is turned off, then the sensor will report the ON status till it is reset (either by XRES or power cycle).
Best regards,
Hari
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Hari,
Thanks for your response !
The object is a cylinder (diameter = 16mm and height around 3mm). I was thinking about making round button with a diameter of 10mm. Should be enough ? My overlay will be 4 to 5mm.
I want to use 8 buttons at the same time.
Best regards,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @ltdndt
Detection of this through a 4 mm overlay would be difficult. Is the cylinder going to be placed vertically (i.e. the 3mm base resting on the sensor) or horizontally, with the longer side on the sensor? With the 3 mm base on the sensor, it would not be possible to detect this.
Can you move to the PSoC MCU line of devices so that we have manual tuning controls?
Best regards,
Hari
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @Hari ,
The longer side will be placed against the overlay.
Like that :
Don't we have manual tuning with the CY8CMBR3110 as well ? I wanted to set the threshold myself and disable the auto tuning. I wanted to use EZ-Click.
What family of PSoC do you recommend ? Is the software development easy to do ? We have to use PCoS Creator, is that right ?
Best regards,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @ltdndt
The longer side being present on the sensor is definitely advantageous.
Don't we have manual tuning with the CY8CMBR3110 as well ? I wanted to set the threshold myself and disable the auto tuning. I wanted to use EZ-Click.
No, we can only set the thresholds in MBR3. We cannot tune the sensors manually or adjust the gain in this device.
I would recommend PSoC 4 - specifically the 4000S device as it contains a newer CapSense IP with better coverage of such corner cases. The software development is easy and we have a lot of code examples to get you started with the design.
Yes, PSoC creator is the right platform for application development.
Best regards,
Hari