- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
greetings,
AnjanaM_61SaEa_4705941broadcomwiced-adminMichaelF_56
i am using CYBT-413055-02 custom module and i am using modus tool box 2.1 and sdk version <version>2.6.0.7989</version>.
i can able to enter into debugging mode using SEGGER JLINK plus and configured SWD pins clock and Data pins.
but when i run the program, the program is not running for example if i run hello sensor code..bluetooth does not advertise.
when i pause the debugger , it goes directly to BUSY_WAIT_TILL_MANUAL_CONTINUE_IF_DEBUG_ENABLED(); to this macro and every time i pause the program, it does not come out of it.
i made the spar_debug_variable=1 to non zero but still its not running.
but when i tried command line debugging it works when i do the following steps,
1. started the jlinkgdb server in the desktop and waiting for GBD connection.
2. then started C:\Users\danny\ModusToolbox\tools_2.1\gcc-7.2.1\bin\arm-none-eabi-gdb.exe and ran the arm-none-eabi-gdb.exe file.
3. typed commands like
target remote localhost:2331
symbol-file (the ELF PATH IN MY COMPUTER)
monitor halt
set var spar_debug_continue=1
s
}
l
continue
4. if i followed the above steps , i can able to run the program once..cant reset or put breakpoints.
please i need help with debug in modus tool box.
thanks and regards,
danny.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Thanks for sharing in community.
Bear with us for a bit more as we are continuing to find the best resolution for you.