ModusToolbox™ Forum Discussions
ModusToolbox™ v3.2 is now available for installation using the new ModusToolbox™ Setup program. ModusToolbox™ provides an adaptable work environment with options for various IDEs, command-line tools with GUI options, and a make-based build system.
ModusToolbox™ v3.2 introduces the following new features:
- New installation process, providing easy access to the core tools and management of optional feature packs.
- The bundled Eclipse IDE for ModusToolbox™ has been updated to leverage Eclipse Platform v4.28, bringing modern OS features and support for Modus-Shell integration in Windows 11.
- Intellisense support has been improved within the Eclipse IDE for ModusToolbox™.
- The underlying ModusToolbox™ build system has been enhanced to improve the overall build performance, by caching project discoverability and build command preprocessing.
- Updated ModusToolbox™ Configurators and Middleware libraries with improved support for 5th Generation CAPSENSE™ devices.
- Usability improvements within the BSP Assistant and Smart I/O tools, providing easier access to key documentation and workflows.
The ModusToolbox™ ecosystem now includes the ModusToolbox™ Setup program (v1.0). This installation tool is the recommended way to install ModusToolbox™ including additional patches and packs.
This setup program is an online installation utility that requires an active internet connection. If you need to download and install ModusToolbox™ in an offline fashion, please refer to the ModusToolbox™ Offline Installation page for details.
Refer to the Release Notes for specific details on the latest product enhancements.
To learn more and download today, visit the ModusToolbox software product page.
Key links:
- ModusToolbox™ Software overview
- ModusToolbox™ Setup program from Infineon Developer Center
- Installation Guide
- User Guide
- Release Notes
We used the custom MTB flow for our own code in MTB 2.4:
git@bitbucket.org:{ORG}/{REPO}#{BRANCH}#$$ASSET_REPO$$/{REPO}
This worked fine in 2.4, make getlibs would pull them all in.
But in MTB 3.2 we get:
mtbquery: could not load ModusToolbox environment information
mtbquery: error creating asset request from file '../deps/repo.mtb' - the first part of the url, 'git@bitbucket.org:{ORG}/{REPO}' is not a valid URI
git can use those from the command line with no passwords, postinstall has been run, and CY_TOOLS_PATHS is set.
- Do I need to fix and how: could not load ModusToolbox environment information?
- Is SSH for git now unsupported?
Show Less
I'm exploring the CSX Touchpad Tuning sample application using the PSoC4 MAX Pioneer kit. In the user manual for the CAPSENSE Tuner app, it says "The middleware supports simultaneous detection up to three touches for a CSX touchpad
touch, so the touch table displays all the detected touches." However, I can only get two touches to show in the CSX Touch Table on the Touchpad View in the Tuner app. I can see the third (and when appropriate, fourth) finger in the main Widget View graphic, but notice only two of the fingers have a colored "dot" in the middle representing the centroid of the touch. I suspect I need to modify the number of centroids that are being tracked and/or reported, but am not sure what parameter I need to change in the capsense_defines header file to do this.
Also, what is the nature of the limitation of the middleware only supporting three simultaneous touches? Is there a theoretical limit of touches CAPSENSE can support?
Show LessHello All,
I wish to use the ModusToolbox for Machine Learning as I plan to get started with ML on Infineon hardware, however, I have a few queries.
- I understand it is supported only for PSoC 6. If there are any others, please help me with the details.
- The hardware/development kits for PSoC 6 are as mentioned in this link but I am not sure if all of these are supported for Machine Learning.
- Is it supported specifically for CY8CKIT-062S4?
- Does ModusToolbox support the application features of imagimob, SensiML and Edge Impulse?
Regards,
Sabat
I'm trying to install ModusToolbox on Linux (Ubuntu 22.04) but I fail to get past the login process.
I originally posted a reply to this thread as it looked similar to my issue but was asked to create a new thread instead.
I downloaded "ModusToolboxSetupInstaller_1.0.0.468_linux_x64.deb" from softwaretools.infineon.com and launched it.
I get the following log messages:
After clicking on "Login" nothing happens and I get the following log:
I don't know how to solve this issue as I don't even see a login prompt. I only get the error "Error: Failed to Login: 'process failed to start'"
Show LessHello, World!
I am trying to install ModusToolbox and am getting the error message
Error: Failed to Login: "Network Error occurred": 'ContentNotFoundError'
Steps to reproduce:
1) Download and install the developer center launcher
2) Launch ModuxToolbox Setup
At this point the software gives the error message
At this point, it doesn't matter if I click "Login" or click on "ModusToolbox Tools Package". Login doesn't even ask me for a username. I get the same error message and "Next >" never becomes enabled.
Any help would be appreciated.
Show LessHello. I have just brought up the CYW920829M2EVK-02 board and was able to build hello world sample code using VS Code. Do you have any sample code for the PDM Mic on-board?
Show Less1、The modus Version: 3.2.0 2、'
2、I create a New application ,the procedure as below
the chip change to “CY8C4025LOI-T412” ,the clolk change from 48MHZ to 24 MHZ which was operated as the notes show //-->compile ok
The CY8C4025LOI-T412 project has 4 Buttons(P2.0 、 P2.3、 P2.4、 P2.5) and a I2C(P3.2 P3.3) that is different from the defaut prorammer .yet the progammer is changed //---compile error
#error The CAPSENSE(TM)Configurator requires anewer version of the CAPSENSE(TM)Middleware. Update the CAPSENSE(TM)Mddleware in your project.
........
#error #CY CAPSENSE BUTTON SELF CAP CLICKmain.c:176:26:error:TIMEOUT MAX VALUE'undeclared(first use in this function)
----------------------------------------------
Project-Doesn-t-Reflect-Middleware-Version-Selected-Using-BSP-Assistant 这个我不明白写的啥,按照这个操作也解决不了 .the URL could not solve my problem
My number :17317187679
Thanks
Show LessHi all,
I would like to try the firmware upgrade example for my dev kit. But it is not working.
Can you please advise me what I have wrong?
I am attaching an error log.
PS: I am using latest ModusToolbox v 3.2.
Best Regards
Koumak
Show LessHi Infineon.
PSoC Creator allows flash protection with “Design Wide Resources(Flash Security)”.
Please confirm below figure.
Could you please let us know how to apply protection to flash in Modus?
Target device is PSoC4100S Max
PSoC4100S Max only supports Modus.
Best Regards.
YuMa
Show LessHi Folks,
From the previows discussion, finally I could download Setup1.0
https://community.infineon.com/t5/ModusToolbox/Release-Announcement-ModusToolbox-v3-2-available-for-download/td-p/714363
Then when I tried to ModusToolbox setup, it did not went good.
So I removed related files, as far as I could think of, then re-downloaded
ModusToolboxSetupInstaller_1.0.0.468_windows_x64_signed.exe
launcher2_2023.9.1_Windows_x32-x64.exe
I installed both and in the Launcher I can see the SETUP
In this window, I'm already logged in as me, but allow me to hide my working mail address 😉
(At least "Log out" icon is there)
Then when I click and start the Setup, I get
Error: Failed to start Launcher Service: 'process failed to start'
and
Error: Failed to check for the ModusToolbox Setup update
Since the upper left of the ModusToolbox Setup 1.0 is saying "Login"
I clicked the "Login" Icon, then got
Error: Failed to Login: 'process failed to start'
Note: The right side of the "Login" Icon is saying "Login session is in progress" >_<
Just in case, let me note that I can login to both MyInfineon and IDC.
(1) MyInfineon
(2) Infineon Developer Community (So, I can post this here)
Since the Setup Utility has removed my ModusToolbox 3.1,
currently I have no MTB on my PC, I'd really like to install v3.2.
Now my question is would someone teach me what the safest or the most reliable way to install MTB v3.2 is?
And/or how can I find the cause(s) of errors above?
moto
Show Less