ModusToolbox™ Forum Discussions
ModusToolbox™ v3.2 is now available for installation using the new ModusToolbox™ Setup program. ModusToolbox™ provides an adaptable work environment with options for various IDEs, command-line tools with GUI options, and a make-based build system.
ModusToolbox™ v3.2 introduces the following new features:
- New installation process, providing easy access to the core tools and management of optional feature packs.
- The bundled Eclipse IDE for ModusToolbox™ has been updated to leverage Eclipse Platform v4.28, bringing modern OS features and support for Modus-Shell integration in Windows 11.
- Intellisense support has been improved within the Eclipse IDE for ModusToolbox™.
- The underlying ModusToolbox™ build system has been enhanced to improve the overall build performance, by caching project discoverability and build command preprocessing.
- Updated ModusToolbox™ Configurators and Middleware libraries with improved support for 5th Generation CAPSENSE™ devices.
- Usability improvements within the BSP Assistant and Smart I/O tools, providing easier access to key documentation and workflows.
The ModusToolbox™ ecosystem now includes the ModusToolbox™ Setup program (v1.0). This installation tool is the recommended way to install ModusToolbox™ including additional patches and packs.
This setup program is an online installation utility that requires an active internet connection. If you need to download and install ModusToolbox™ in an offline fashion, please refer to the ModusToolbox™ Offline Installation page for details.
Refer to the Release Notes for specific details on the latest product enhancements.
To learn more and download today, visit the ModusToolbox software product page.
Key links:
- ModusToolbox™ Software overview
- ModusToolbox™ Setup program from Infineon Developer Center
- Installation Guide
- User Guide
- Release Notes
Still getting used to the newer ModusToolbox apps, as we had used PSoC Creator for years. I created a new project based on the MPN using the BSP Assistant app. This project uses the CapSense library to create a touchpad. Using the CapSense Configurator app, I successfully assigned each of the Rows/Columns to a specific GPIO. This assignment was reflected in the Device Configurator app. However, now I would like to add a few more rows/columns to my touchpad. I labelled these GPIO in the "Pins" tab of the Device Configurator. However, these new GPIO don't appear in either the Device Configurator under the Peripherals>System>CapSense>MSC 0 Parameters window, nor do they appear in the CapSense Configurator under Scan Configuration> Pin. It almost seems like I am missing a step of either importing the Device Config to the CapSense Configurator or vice versa.
Here you can see I have configured the pin at Port 5, Pin 6 same way as the others and named it E45:
But when I then go to the Peripherals tab and try to assign Row 7 to it, it does not appear in the drop-down list:
If I check the CapSense Configurator, it also does not appear in the drop-down list:
None of the rest of the GPIO that I added show up either. What am I doing wrong?
Show Less
Hi Folks,
From the previows discussion, finally I could download Setup1.0
https://community.infineon.com/t5/ModusToolbox/Release-Announcement-ModusToolbox-v3-2-available-for-download/td-p/714363
Then when I tried to ModusToolbox setup, it did not went good.
So I removed related files, as far as I could think of, then re-downloaded
ModusToolboxSetupInstaller_1.0.0.468_windows_x64_signed.exe
launcher2_2023.9.1_Windows_x32-x64.exe
I installed both and in the Launcher I can see the SETUP
In this window, I'm already logged in as me, but allow me to hide my working mail address 😉
(At least "Log out" icon is there)
Then when I click and start the Setup, I get
Error: Failed to start Launcher Service: 'process failed to start'
and
Error: Failed to check for the ModusToolbox Setup update
Since the upper left of the ModusToolbox Setup 1.0 is saying "Login"
I clicked the "Login" Icon, then got
Error: Failed to Login: 'process failed to start'
Note: The right side of the "Login" Icon is saying "Login session is in progress" >_<
Just in case, let me note that I can login to both MyInfineon and IDC.
(1) MyInfineon
(2) Infineon Developer Community (So, I can post this here)
Since the Setup Utility has removed my ModusToolbox 3.1,
currently I have no MTB on my PC, I'd really like to install v3.2.
Now my question is would someone teach me what the safest or the most reliable way to install MTB v3.2 is?
And/or how can I find the cause(s) of errors above?
moto
Show Less
Hi Infineon.
PSoC Creator allows flash protection with “Design Wide Resources(Flash Security)”.
Please confirm below figure.
Could you please let us know how to apply protection to flash in Modus?
Target device is PSoC4100S Max
PSoC4100S Max only supports Modus.
Best Regards.
YuMa
Show LessHi all,
I would like to try the firmware upgrade example for my dev kit. But it is not working.
Can you please advise me what I have wrong?
I am attaching an error log.
PS: I am using latest ModusToolbox v 3.2.
Best Regards
Koumak
Show LessI would like to use Modustoolbox to develop rt thread project and was trying to follow the guide https://community.infineon.com/t5/Knowledge-Base-Articles/Porting-RT-Thread-to-ModusToolbox/ta-p/664401
While the guide is awesome demonstrating rt thread works, It does not have enough details of steps and setup for me.
I tried creating a capsense project, import rt thread into the project, removed all unnecessary srcs. But I got stuck with many weird libc & toolchain errors with the default gcc-arm compiler on Linux, like time_t is unknown typename and false/true/bool is undefined.
This first error is kinda "fixed" by explicitly telling eclipse to include the newlib header dir. The second is not. It is really weird and the IDE can successful locate those headers.
Could anyone help me out with this?
Show LessModusToolbox™ v3.2 is now available for installation using the new ModusToolbox™ Setup program. ModusToolbox™ provides an adaptable work environment with options for various IDEs, command-line tools with GUI options, and a make-based build system.
ModusToolbox™ v3.2 introduces the following new features:
- New installation process, providing easy access to the core tools and management of optional feature packs.
- The bundled Eclipse IDE for ModusToolbox™ has been updated to leverage Eclipse Platform v4.28, bringing modern OS features and support for Modus-Shell integration in Windows 11.
- Intellisense support has been improved within the Eclipse IDE for ModusToolbox™.
- The underlying ModusToolbox™ build system has been enhanced to improve the overall build performance, by caching project discoverability and build command preprocessing.
- Updated ModusToolbox™ Configurators and Middleware libraries with improved support for 5th Generation CAPSENSE™ devices.
- Usability improvements within the BSP Assistant and Smart I/O tools, providing easier access to key documentation and workflows.
The ModusToolbox™ ecosystem now includes the ModusToolbox™ Setup program (v1.0). This installation tool is the recommended way to install ModusToolbox™ including additional patches and packs.
This setup program is an online installation utility that requires an active internet connection. If you need to download and install ModusToolbox™ in an offline fashion, please refer to the ModusToolbox™ Offline Installation page for details.
Refer to the Release Notes for specific details on the latest product enhancements.
To learn more and download today, visit the ModusToolbox software product page.
Key links:
- ModusToolbox™ Software overview
- ModusToolbox™ Setup program from Infineon Developer Center
- Installation Guide
- User Guide
- Release Notes
ModusToolbox补丁安装指南
补丁及文档请从此贴附件中下载
- 安装ModusToolBox 3.1 (ModusToolbox_3.1-windows-install.exe)
请注意: 安装时请选择install for me only , 保持默认安装路径
- 运行 windows Power Shell (Admin管理员身份)
3. 请按顺序输入以下指令(Admin管理员身份)
- 安装补丁脚本 (Admin管理员身份)
- 打开 ModusTool Box TM 开发环境,开启创意之旅
Dear forum,
I have a problem uninstalling Modus Toolbox Software 3.2.0.16028.
The situation:
I installed the ModusToolbox Setup 1.0.0 and Modus Toolbox Dashboard 3.2 from the Infineon website.
However, I had a problem with opening the Eclipse ID because the name of my root folder consists of 2 words with space in between.
So I uninstalled the Dashboard. Doing so I had issues with my antivirus software and the deinstallation.
Any way I changed the name of my root folder not to have a space between the 2 words.
I installed the Modus Toolbox Dashboard.
I still could not access the Eclipse part of the program because it seemed to remember the problem with the root folder name although it had been changed.
I wanted to uninstall the Modus Toolbox Dashboard however, the uninstall software had been deleted by my antivirus for security reasons.
So I am stuck.
Tried uninstalling it from Windows Settings/Apps but was not able. The uninstall icons not clickable.
Do you have a solution or workaround?
Thanks,
Jedison
Show LessHi,
Whenever I open a MTB project, I get a command line terminal getting launched as well. Is there a way to fix this issue? I am using MTB v3.0.
I am attaching the video captured.
Thank you.
Balek
Show LessI cannot complete installation of ModusToolbox. It says that Login is required to complete installation, but login fails. This is with ModusToolbox Setup 1.0, just downloaded.
It says Login session is in progress ... then
Error: Failed to Login: 'Network Error occurred: 'OperationCancelledError"
Why is the login failing and how do I correct this?
Show Less