Bluetooth SDK

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
FeTa_4356966
Bluetooth SDK
Hi I have paired the Bluetooth SPP profile with smartphone.After disconnection, can I initiate a reconnection from the device side?Can wiced_bt_spp_co... Show More
gykim
Bluetooth SDK
I'm trying to reset by software. void (*reset)(void); reset = (void(*)())0x200000; reset();   It is not working. Can you explain why it doesn't ... Show More
KeTa_1341526
Bluetooth SDK
Hello, The ModusToolbox (mtb) Bluetooth SDK provides the HRC / HRS Library API for use with the Heart Rate Profile (HRP). I would like to develop a pr... Show More
HyJe_4673431
Bluetooth SDK
Hello, I want to search BR/EDR devices which use limited inquiry access code. It seems like that setting 'mode' paramter in wiced_bt_dev_inq_parms_t t... Show More
kf
Bluetooth SDK
Please help me to understand how to implement the following scenario: my device based on CYW20706 is BLE peripheral that is able to accept pairing fro... Show More
niels5750
Bluetooth SDK
Hi, we are doing an ble mesh application using CYBT-483056-02. In the  Vendor Specific example it is possible to set the tx power (wiced_bt_mesh_core_... Show More
anje_2248446
Bluetooth SDK
Hello Cypress, I have cyw20719b2 SDS Sleep configuration with TRASNPORT / NO_TRANSPORT mode. Device goes to SDS Sleep correctly. But after around 3 mi... Show More
kf
Bluetooth SDK
I'm trying to generate Bluetooth project for CYW920706WCDEVAL with ModusToolbox 2.4 and it fails for any project I select. The project's directory get... Show More
anhnhancao
Bluetooth SDK
Dear all, I have a CYW920721B2 Evaluation Board and want to run the Audio_Headset_and_Speaker Example on ModusToolbox IDE, The point is that i want to... Show More
eSteve
Bluetooth SDK
Hi, in the WICED BT SDK v3.1 I see a call back defined for the SPP BT Tx being completed: wiced_bt_spp_tx_complete_callback_t    WICED CYW208XX: SPP Library API (infineon.github.io)... Show More