Bluetooth SDK

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
gykim
Bluetooth SDK
I'm trying to reset by software. void (*reset)(void); reset = (void(*)())0x200000; reset();   It is not working. Can you explain why it doesn't ... Show More
gykim
Bluetooth SDK
I'am trying to ble_mouse source on custom board with cyw20819. For idle status, I got the 'HCI_ERR_INSTANT_PASSED' for connection_down reason. I mean ... Show More
marzuniga845
Bluetooth SDK
Hello all, I have a the CYBT-213043-MESH board, and my question is this: Would it be possible to have a single application with both client and server... Show More
kf
Bluetooth SDK
Please help me to understand how to implement the following scenario: my device based on CYW20706 is BLE peripheral that is able to accept pairing fro... Show More
gykim
Bluetooth SDK
I can't find releasev3.2.0 in github https://github.com/Infineon/wiced_btsdk. How can I get btsdk 3.2 without modustoolbox? Regards, gykim Show More
rodneydavies
Bluetooth SDK
Hello,   Could someone please let me know where I could obtain SDK and other programming manuals/materials/software for programming the firmware on th... Show More
lei
Bluetooth SDK
I tested 20719 audio_watch demo. It can be successfully paired and connected with Bluetooth speakers. However, when the Bluetooth speaker initiates a ... Show More
eSteve
Bluetooth SDK
I have a query with respect to the parameters of the operation wiced_bool_t wiced_bt_spp_send_session_data( uint16_t handle, uint8_t * p_data, uint32_... Show More
niels5750
Bluetooth SDK
Hi, we are doing an ble mesh application using CYBT-483056-02. In the  Vendor Specific example it is possible to set the tx power (wiced_bt_mesh_core_... Show More
eSteve
Bluetooth SDK
Hi, in the WICED BT SDK v3.1 I see a call back defined for the SPP BT Tx being completed: wiced_bt_spp_tx_complete_callback_t    WICED CYW208XX: SPP Library API (infineon.github.io)... Show More
Forum Information

Bluetooth SDK

Discussion forum regarding ModusToolbox with the AIROC™ Bluetooth SDK topics.
Top liked authors