Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Bluetooth SDK

Recent discussions

Sort by:
HeDi_4635501
Bluetooth SDK
Hi, I have a CY8CKIT-062-WIFI-BT board and would like to read temperature values from another controller (ESP32 conroller+BME280Sensor), for example.... Show More
HereturbiesWalt
Bluetooth SDK
I am having trouble with extracting a .tar.gz file and accessing its files on a docker image. I've tried looking around Stackoverflow, but the solutio... Show More
tayo
Bluetooth SDK
Hello Infineon support team.   We are evaluating a sample application "Audio_Headset_and_Speaker" using CYW920721B2EVK-02. <Board configuration>-CYW9B... Show More
ChCh_3584941
Bluetooth SDK
We are using the HCI UART of the CYW20719B2 chip in Raw Mode.   We have the communication working , but have noticed that there is a delay of ~ 50ms f... Show More
RoMc_863046
Bluetooth SDK
I am using the EZ-Serial Host API Protocol Library with the CYBT-343026-01. App: 1.2.29 build 29Stack: 5.2.0 build 22Protocol: 1.3HW: CYBT-343026-01 I... Show More
u8
Bluetooth SDK

测试发现频率高了100K左右,请问CYW20706内部是否有可调整电容能够调整频率的?

14993901
Bluetooth SDK
Hi, 编程环境ModusToolbox,芯片cyw20719b2,运行于BLE server状态,(1)程序片段如下:APPLICATION_START(){...pImgSemaphore = wiced_rtos_create_semaphore();//线程同步信号量wiced_rtos_i... Show More
arwhalley
Bluetooth SDK
I am evaluating the CYW20706 and the AIROC solutions as a replacement for our existing IoT Bluetooth functionality. It is essential for the operation ... Show More
KeTa_1341526
Bluetooth SDK
Hello,   I would like to use Quad SPI Master with CYBT-413061-02 (CYW20721). I plan to use the Modus Tool Box / Bluetooth SDK.   However, in the 20719... Show More
anhnhancao
Bluetooth SDK
Dear all, I already own a CYW20706B2 Evaluation KIT. I want to connect it to an Audio codec and use the share-clock feature on CYW20706(GPIO BT_CLK_RE... Show More