Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Bluetooth SDK Forum Discussions

Bluetooth SDK Forum Discussions

Sort by:
kartheek_adivi
Bluetooth SDK
Hi, I'm using CYW20721. My application which supports OTA is around 750Kb. Since the total internal flash is 1Mb, I think it's not possible to do a OT... Show More
MaKo_4657646
Bluetooth SDK
In SPP, if the MTU of the connection destination is small, that value will be used.Therefore, it seems that the length sent by wiced_bt_spp_send_sessi... Show More
AnBe_1519071
Bluetooth SDK
A project developped inside ModusToolBox for CYBT-423054-02 can run on a CYBT-423028-02? If not, how can I develop a prject for CYBT-423028-02 inside ... Show More
KeTa_1341526
Bluetooth SDK
Hello, We are developing CYBT-483056-02 with MTB2.2. On CYBT-483039-02 with CYW20719B1, it was necessary to add the following settings in WICED. https://community.cypress.com/t5/WICED-Smart-Bluetooth/CYBT-483039-02-documented-PA-LNA-control-interface/td-p/142176... Show More
JiNg_296976
Bluetooth SDK
Hi there, I prepare the mesh network based on the AN227069 - Use Case #1: Dimmer Switch ControllingThree Dimmable Light Bulbs. Everything was perfectl... Show More
wizzbert
Bluetooth SDK
While trying to build the "empty_project", I get a build error that it can not link to the elf file. Build output is attached.  It is not building the... Show More
MaCh_4826131
Bluetooth SDK
Hi, I have a microphone connected to my CYW920819 board via i2s. Unfortunately I am unable to get it to stream to my bt headphones via a2dp (is it eve... Show More
paddlesteamer
Bluetooth SDK
Hello, I want to send data via I2S DOut channel to an audio codec chip on the CYW920819EVB-02 board but I couldn't find a way to do it. I'm looking at... Show More
SnGh_4568476
Bluetooth SDK
Hello Team, I am using CYW20819 board and mesh controller app for my application. I observe in app that when device or module advertise it shows devic... Show More
ChCh_3584941
Bluetooth SDK
Can you point me to any examples for enabling PDS and SDS Sleep for the CYW20179B2 chip for ModusToolBox V2.1 SDK Version 2.7.1?  Or to a comprehensiv... Show More