- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I want to use CYW20737 for bluetooth connection.I m getting confused between WICED and Modus Toolbox.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi suja_4727136 ,
Its different SDKs. If you go through the release notes , you will get the supported devices info.
CYW20737 is supported on WICED SMART SDK available here :
https://www.cypress.com/products/wiced-software
Thanks & Regards,
Anjana
Other useful references :
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi suja_4727136 ,
Its different SDKs. If you go through the release notes , you will get the supported devices info.
CYW20737 is supported on WICED SMART SDK available here :
https://www.cypress.com/products/wiced-software
Thanks & Regards,
Anjana
Other useful references :
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
This admittedly can be confusing, so I wanted to clarify here for the benefit of everyone that may have the same question.
These two spaces point to the same WICED WWD-based (underlying driver) SDK, which supports both WiFi and Bluetooth today (WICED Studio Wi-Fi/Combo Docs & Downloads😞
CYW20706
CYW20819
CYW20719B1
CYW20735
Certified non-PSOC BT Modules based on the silicon above
BT
CYW20706
CYW20819
CYW20719B1
CYW20735
Certified non-PSOC BT Modules based on the silicon above
WiFi and WiFi/Combo:
With STM32F:
CYW43362
CYW43364
CYW4343W/CYW43438
CYW43340
With onboard Cortex R4
CYW43907/CYW54907
The following is another version of the WICED development flow which supports the CYW20732/20736 and 20737 ONLY: WICED Smart Docs & Downloads
-Note here that the 20732 uses version 1.x while the 20736/37 use version 2.x (different firmware in each device, so the SDKs are not interchangeable).
-The CYW20732/6/7 is not supported within ModusToolbox Bluetooth SDK
In addition, there was an early version of the WICED "SmartReady" SDK which supported only the CYW20706/07. That version was released to a few early adopters only as the same functionality was eventually migrated into WICED Studio.
Above comprises our legacy SW offering.
WICED Studio will continue to be supported on the WiFi/Combo side with patches and security fixes. The Bluetooth functionality within WICED Studio will migrate (has migrated) to the ModusToolbox Bluetooth SDK. The most recent version of the WICED Smart SDK was released in 2016 and there are no plans to release new versions of this SDK.
Moving forward, our Cortex M-Class development flow will be ModusToolbox based using WHD (underlying driver):
Bluetooth
Bluetooth SDK 2.6 Technical Brief (lists chips and development platforms)
WiFi/Combo with PSoC 6 host:
Again, the discussion above is M-Class based. We will also continue to support Cortex A class processors with our FMAC Linux based driver, which is available here: Wi-Fi/Bluetooth for Linux .
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1. Thanks MichaelF_56 for the elaborated reply.
As you said "The Bluetooth functionality within WICED Studio will migrate (has migrated) to the ModusToolbox Bluetooth SDK.", So I will go with code development in ModusToolbox. Thanks for that clarification.
2. I m not able to open TEST ModusToolbox Bluetooth SDK link, it takes me to a page which says "Unauthorized".
3. There is no mention of CYW20737 or its development board BCM92073X_LE_TAG4 in Bluetooth SDK 2.6 Technical Brief
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi SuJa_4727136 ,
Only WICED studio chips are migrated to Modus.
CYW20737 is not supported in WICED Studio or Modus. It is only supported in WICED Smart SDK.
Regards,
Anjana
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
The fixed the broken link above.