- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear all,
I have a CYW920721B2 Evaluation Board and want to run the Audio_Headset_and_Speaker Example on ModusToolbox IDE,
The point is that i want to extend the MTU size of BLE connection to 247 (Default is 23 byte). I've read some answers on Cypress forum and they recommend to edit "gatt_cfg.max_mtu_size" and also call wiced_bt_gatt_configure_mtu() API when the BLE connection is established to reconfig the MTU size.
I changed gatt_cfg.max_mtu_size to 247 and call wiced_bt_gatt_configure_mtu(p_status->conn_id, 247) inside hci_control_le_connection_up() but it always return 0x80 (WICED_BT_GATT_NO_RESOURCES).
I really appreciate if any one could help me to config the MTU size correctly.
Solved! Go to Solution.
- Labels:
-
ModusToolbox Bluetooth SDK
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @anhnhancao ,
Sorry I am late. Not sure if you already fixed this. Let me explain the usage
- On your Peripheral , you can set the MTU size by modifying config file as you already know. For example,
.gatt_cfg = /* GATT configuration */
{
.appearance = APPEARANCE_GENERIC_TAG, /**< GATT appearance (see gatt_appearance_e) */
.client_max_links = 2, /**< Client config: maximum number of servers that local client can connect to */
.server_max_links = 1, /**< Server config: maximum number of remote clients connections allowed by the local */
.max_attr_len = 244,
.max_mtu_size = 247
},
- By default a BLE connection will use MTU size of 23. If you have to use a higher value their either of the two devices should send MTU exchange request. Then the negotiated MTU value (smallest among both) will be used for further communication.
- In your application if Central device is capable of sending a mtu exchange request, then that is good enough. You need not have to call wiced_bt_gatt_configure_mtu API again in Cypress Peripheral BT device.
In the other case , if you want to initiate this from cypress BT side, then use the API wiced_bt_gatt_configure_mtu. Inorder to use this API , in config file you should have entered a non zero value for .client_max_links under .gatt_cfg
Please try this method and let us know if you face any issues.
Regards,
Anjana