Hello!
Could you tell me if there is any API for programmable chip shutdown from the application level?
Solved! Go to Solution.
What do you mean by turn off? In the application, you can only set the device to SDS mode which is the lowest power mode. You can refer to the following AN: CYW20706, CYW20735, and CYW20719 Low-Power Modes (cypress.com)
If you want to totally turn off the device, you need to shut down the power supply.
What do you mean by turn off? In the application, you can only set the device to SDS mode which is the lowest power mode. You can refer to the following AN: CYW20706, CYW20735, and CYW20719 Low-Power Modes (cypress.com)
If you want to totally turn off the device, you need to shut down the power supply.
Ok, thank you!
Could you please tell us if SDS and HID-OFF modes are supported for CYW720719B2 in the current SDK?
Yes, it is supported in the Modus and BTSDK tools.