Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
jama_4535901
Level 3
Level 3
10 sign-ins 5 sign-ins 25 replies posted

Hello

I am using modus toolbox

I want to know how I can print in WICED UART Peripheral the united identifier ID of the CYBT-233043-02

I used the mac address as an identifier but it always changes every time a new network is created, I want to know if the unique identifier ID never changes

or what unique identifier has each module cybt-213043-02, that never changes, that is from the factory, and how can I print it on WICED UART?

0 Likes
1 Solution
DheerajPK_41
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi,

You can set BT device address for your BT device in the makefile of the application. Change BT_DEVICE_ADDRESS to an appropriate address. Is this what you are looking for?

BT_DEVICE_ADDRESS?=default

The BT address is 6 bytes, for example 20819A10FFEE. By default, the SDK will set a BDA for your device by combining the 7 hex digit device ID with the last 5 hex digits of the host PC MAC address.

Thanks,

-Dheeraj

View solution in original post

0 Likes
6 Replies
DheerajPK_41
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi,

You can set BT device address for your BT device in the makefile of the application. Change BT_DEVICE_ADDRESS to an appropriate address. Is this what you are looking for?

BT_DEVICE_ADDRESS?=default

The BT address is 6 bytes, for example 20819A10FFEE. By default, the SDK will set a BDA for your device by combining the 7 hex digit device ID with the last 5 hex digits of the host PC MAC address.

Thanks,

-Dheeraj

0 Likes

We are going to buy 4000 CYBT-213043-02 modules, BUT I DO NOT WANT TO BE LOADING DIFFERENT CODES WITH THE ABT_DEVICE_ADDRESS LINE modified, it is tedious for us,

I want use an ID or some identifier that the BLE module already has as an example what is mentioned in this thread How to get PSOC 6 device ID or something unique id to differentiating chip

but I want to get a factory identifier that has each module as the factory ID or something like that for CYBT-21304-02,

0 Likes

Hi jama_4535901 ,

There is no Unique ID for 20xx based devices like PSoC devices. The only way is - you can set unique BD address to each modules during production programming time at your side as DheerajP_41  suggested.

Regards,

Anjana

0 Likes

I understand

I will have to assign an identifier with the device number and the name( Network name) of the network

when I create a network with MeshClientControl APP for example Mesh Name: RED1 (as shown in the image)

and then provision the other nodes

in the provisioning code client / vendor client, where the network name is stored: RED1

Where can I get the network name: RED 1 in the code? to print it with the line

WICED_BT_TRACE ("MESH NAME:% B \ n", saved_mesh_name);

I tried to find where the Network name is saved but I can't find it in the code in Modustoolboxnetwork.PNG

0 Likes

Hi,

The network name is stored in the JSON file which is the database of the provisioner. You will have to read it from it.

Please check mesh_client_lib/meshdb.c for implementation of routines for database operations.

Thanks,

-Dheeraj

I try that the code vendor specific prints the name of the network with a function that I add in the code mesh_client_lib / meshdb.c as shown in the image, but it is not working,

Could you help me?

MESHNAME.PNG

0 Likes