Hello!
I use an example from the AG library and I can't connect a wide-band headset to my application.
Narrow band headsets work fine - there is audio.
But when I connect the wideband - there is no audio.
Would you like to see if I am using the wrong settings? Or the chip simply does not support the wideband?
/*
* Create SCO connection as an originator or an acceptor
*/
void hfp_ag_sco_create( hfp_ag_session_cb_t *p_scb, BOOLEAN is_orig )
{
//wiced_bt_dev_status_t status;
wiced_bt_sco_params_t params = hf_control_esco_params;
/* remove listening SCO */
if ( p_scb->sco_idx != BTM_INVALID_SCO_INDEX )
wiced_bt_sco_remove( p_scb->sco_idx );
/* Attempt to use eSCO if remote host supports HFP >= 1.5 */
if ( is_orig )
{
if (p_scb->retry_with_sco_only)
{
p_scb->retry_with_sco_only = WICED_FALSE;
params.packet_types = BTM_SCO_LINK_ONLY_MASK;
}
else
{
#if (BTM_WBS_INCLUDED == TRUE)
if ( p_scb->peer_supports_msbc && !p_scb->msbc_selected )
{
/* Send +BCS to the peer and start a 3-second timer waiting for AT+BCS */
hfp_ag_send_BCS_to_hf (p_scb);
wiced_start_timer (&p_scb->cn_timer, 3);
return;
}
/* If WBS is negotiated, override the necessary defaults */
if ( p_scb->msbc_selected )
{
params.use_wbs = WICED_TRUE;
params.max_latency = 13;
params.retrans_effort = BTM_ESCO_RETRANS_QUALITY;
params.packet_types = ( BTM_SCO_PKT_TYPES_MASK_EV3 | /* EV3 + 2-EV3 */
BTM_SCO_PKT_TYPES_MASK_NO_3_EV3 |
BTM_SCO_PKT_TYPES_MASK_NO_2_EV5 |
BTM_SCO_PKT_TYPES_MASK_NO_3_EV5 );
BT_Trace(BT_RES_WICED_USE_WBS);
}
else
BT_Trace(BT_RES_WICED_USE_NBS);
#endif
/* Igf setup fails, fall back to regular SCO */
p_scb->retry_with_sco_only = WICED_TRUE;
}
wiced_bt_sco_create_as_initiator( p_scb->hf_addr, &p_scb->sco_idx, ¶ms );
}
else
{
p_scb->retry_with_sco_only = WICED_FALSE;
wiced_bt_sco_create_as_acceptor( &p_scb->sco_idx );
}
WICED_BT_TRACE( "hfp_ag_sco_create is_orig: %u sco_idx: 0x%0x status:0x%x retry_with_sco_only: %u\n",
is_orig, p_scb->sco_idx, status, p_scb->retry_with_sco_only );
}
A small clarification for the question:
Narrow band headsets work fine - PCM is sent off the chip.
But when I connect the wideband - PCM is not sent off the chip.
Hi AlGo_4347736,
The clock settings for both narrow band and wide band are different. Please check PCM/I2S Clock setting in CYW20706 for details on the same.
Thanks! I saw this document.
"This is taken care by the WICED Stack. You just need to enable or disable WBS in the application project" - This is what was done.
I get here by the logs:
if ( p_scb->msbc_selected )
{
params.use_wbs = WICED_TRUE;
params.max_latency = 13;
params.retrans_effort = BTM_ESCO_RETRANS_QUALITY;
params.packet_types = ( BTM_SCO_PKT_TYPES_MASK_EV3 | /* EV3 + 2-EV3 */
BTM_SCO_PKT_TYPES_MASK_NO_3_EV3 |
BTM_SCO_PKT_TYPES_MASK_NO_2_EV5 |
BTM_SCO_PKT_TYPES_MASK_NO_3_EV5 );
BT_Trace(BT_RES_WICED_USE_WBS);
}
Or do you have to change the frequency? How can I do this?
Setting pins:
wiced_hal_gpio_select_function(WICED_P04, WICED_PCM_CLK_I2S_CLK);
wiced_hal_gpio_select_function(WICED_P07, WICED_PCM_OUT_I2S_DO);
wiced_hal_gpio_select_function(WICED_P10, WICED_PCM_IN_I2S_DI);
wiced_hal_gpio_select_function(WICED_P06, WICED_PCM_SYNC_I2S_WS);
Configure the PCM like this:
wiced_hal_pcm_config_t pcmConfig;
memset(&pcmConfig, 0, sizeof(pcmConfig));
pcmConfig.mode = WICED_HAL_PCM_MODE;
pcmConfig.role = WICED_HAL_PCM_MASTER;
pcmConfig.pcm_param.fillData = WICED_HAL_PCM_FILL_0S;
pcmConfig.pcm_param.frame_type = WICED_HAL_PCM_FRAME_TYPE_SHORT;
pcmConfig.pcm_param.lsbFirst = WICED_HAL_PCM_MSB_FIRST;
pcmConfig.pcm_param.rightJustify = WICED_HAL_PCM_ENABLE_RIGHT_JUSTIFY;
wiced_hal_set_pcm_config (&pcmConfig);
With the logic analyzer we have seen that the PCM bit-clock and frame-sync is generated as expected by the BT-chip also in wide-band. PCM samples are also transmitted from the codec to the BT-chip correctly. But for some reason the samples are coded and sent from the BT-chip to the headset. No pcm samples coming from the BT-chip can be seen on the bus. Probably something is missing in the PCM routing inside the BT-chip or codec negotiation with the headset.