Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
wizzbert
Level 1
Level 1
10 sign-ins 5 replies posted 5 sign-ins

For CYW920719B2Q40EVB-01, using ModusToolbox 2.2,


While trying to build the "empty_project", I get a build error that it can not link to the elf file. Build output is attached.

It is not building the elf file for the empty project. I have no idea why or even where to check the specification that it build the elf file.

Full error log attached. Per the help, this should build "out of the box" with no changes and do something simple, but it doesn't. ALL other projects build just fine, this is the ONLY one that doesn't.

>>>

Compiling V:/Software/MedPatch/MedPatchPer/template/empty_wiced_bt/build/CYW920719B2Q40EVB-01/generated/lib_installer.c  -DWICED_BT_TRACE_ENABLE -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1  -DHCI_UART_MAX_BAUD=4000000 -DHCI_UART_DEFAULT_BAUD=3000000 -DSS_LOCATION=0x500000 -DVS_LOCATION=0x501000 -DDS_LOCATION=0x503000 -DDS2_LOCATION=0x582000 -DCYW20719B2=1 -DBCM20719B2=1 -DBCM20719=1 -DCYW20719=1 -DCHIP=20719 -DAPP_CHIP=20719 -DOTA_CHIP=20719 -DCHIP_REV_A_20719B2=1 -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M4 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYW920719B2Q40EVB_01"' -DWICED_SDK_MAJOR_VER=2 -DWICED_SDK_MINOR_VER=5 -DWICED_SDK_REV_NUMBER=0 -DWICED_SDK_BUILD_NUMBER=7341 -g3 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_SOFTFP -DCOMPONENT_bsp_design_modus -DCOMPONENT_gatt_utils_lib -DCOMPONENT_hidd_lib -I. -I../../../dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/COMPONENT_bsp_design_modus -I../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/COMPONENT_bsp_design_modus -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/../../../dev-kit/baselib/20719B2/include -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/../../../dev-kit/baselib/20719B2/include/hal -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/../../../dev-kit/baselib/20719B2/include/internal -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/../../../dev-kit/baselib/20719B2/include/stack -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/../../../dev-kit/baselib/20719B2/internal/20719B2 -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/../../../dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01 -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/../../../dev-kit/btsdk-include -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/WICED -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/WICED/common -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/include -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/include/arm -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/include/arm/cmsis -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/include/hal -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/include/internal -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/include/stack -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/internal -I./../../../wiced_btsdk/dev-kit/baselib/20719B2/internal/20719B2 -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01 -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/../../../dev-kit/baselib/20719B2/include -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/../../../dev-kit/baselib/20719B2/include/arm/cmsis -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/../../../dev-kit/baselib/20719B2/include/hal -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/../../../dev-kit/baselib/20719B2/include/internal -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/../../../dev-kit/baselib/20719B2/include/stack -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/../../../dev-kit/baselib/20719B2/internal/20719B2 -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/../../../dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01 -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/../../../dev-kit/btsdk-include -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/COMPONENT_bsp_design_modus -I./../../../wiced_btsdk/dev-kit/bsp/TARGET_CYW920719B2Q40EVB-01/COMPONENT_bsp_design_modus/GeneratedSource -I./../../../wiced_btsdk/dev-kit/btsdk-include -I./GeneratedSource

    Linking output file EmptyWicedBluetooth.elf

collect2.exe: error: ld returned 1 exit status

make[1]: *** [../../../wiced_btsdk/dev-kit/baselib/20719B2/make/core/build.mk:470: V:/Software/MedPatch/MedPatchPer/template/empty_wiced_bt/build/CYW920719B2Q40EVB-01/Debug/EmptyWicedBluetooth.elf] Error 1

make: *** [../../../wiced_btsdk/dev-kit/baselib/20719B2/make/core/main.mk:350: secondstage] Error 2

"C:/ModusToolbox/tools_2.2/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_MAKE_IDE_VERSION=2.2 CY_IDE_TOOLS_DIR=C:/ModusToolbox/tools_2.2 -j8 all" terminated with exit code 2. Build might be incomplete.

0 Likes
1 Solution
DheerajPK_41
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi,

Ok. So we got the actual issue.

We are working with our dev team to update the offline package;s. We are looking forward to automatically post the offline packages to a public repo along with every new release of software. 

For now, if you don't want to wait till it gets updated, you can use a system with internet connected and select all the apps under 'CYW20719B2Q40EVB-01' (since current project is only with this) platform and do a one time import. Then copy the .modustoolbox cache to your offline development system and follow the instructions in the blog.  https://community.cypress.com/t5/Resource-Library/ModusToolbox-offline-libraries/ta-p/252265 

Thanks,

-Dheeraj

View solution in original post

0 Likes
8 Replies