- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am using the CY-333047 Module with the EZ-Serial Firmware. It's a special purpose configuration (MSP430 communicating directly to the Serial IF with Flow Control). The problem that I'm seeing is that I can easily/consistently transferring 625 bytes of data, BUT if I increase the size of the Buffer over that, I begin timing out receiving the buffer data. The protocol is a simple command-response where I send a command to the device with the size of the response message. The slave receives the command then then sends the size of the response packet, followed by the dataset (a simple saw wave) with the MSP moving the data to the Cypress Radio as fast as it will accept the data (CTS).
What happens is that the many times will timeout before receiving all of the data from the Radio. Below approximately 690 Bytes of Data, no problem but as you go higher, the timeouts begin to occur. It always recovers and we continue BUT I see various amounts of the end of the buffer not making it over and timing out. Making the timeout larger does not fix the problem. The Interface is configured as 500KBaud with Flow Control.
Thanks in advance.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Are you using the classic BT function or BLE function?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Good Morning. That's a good question. I assumed that because I was communicating to a Broadcom BCM20702 Bluetooth 4.0 Device (on Win10) that it would be Legacy/Classic BT. The RFCOMM TDI driver is also loaded, but I can't get much about it either. How do I check which function is being used? I need to use the Classic BT Function.
Regards, Rich
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
When you connect to the device, the device name with a 'BT' suffix is for classic BT. The name without 'BT' suffix is for BLE profile.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for the response. Yes the devices report as EZ-Serial 40:1D:66_BT, so I assume that they are reporting as classic.
So no reconfiguration is required, no?
Are there any limitations on the size of the messages in SPP? Again, after around 625 bytes, I start getting timeouts on the SPP interface.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Could you share some logs about the problem? Does the problem happen with a reconnection?