- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm trying to generate Bluetooth project for CYW920706WCDEVAL with ModusToolbox 2.4 and it fails for any project I select. The project's directory gets created and it is not empty, its content looks OK, but the project does not appear in Project Explorer in ModusToolbox IDE. Also "mtb_shared\wiced_btsdk" directory is empty.
Please find log for "LE Hello Sensor" project below.
Checking if remote manifest is accessible...
Getting manifests from remote server...
Processing super-manifest https://github.com/cypresssemiconductorco/mtb-super-manifest/raw/v2.X/mtb-super-manifest-fv2.xml...
Successfully acquired the information.
Summary:
BSP: CYW920706WCDEVAL
Template Application(s): LE Hello Sensor
Application(s) Root Path: C:/Work/mtw
Press "Create" to create the selected application(s).
Collecting application data...
Info: The following entered on the command line will create the exact same project as that created with the GUI tool:
C:/Infineon/Tools/ModusToolbox/tools_2.4/project-creator/project-creator-cli.exe --board-id CYW920706WCDEVAL --board-uri https://github.com/cypresssemiconductorco/TARGET_CYW920706WCDEVAL --board-commit latest-v3.X --app-id mtb-example-btsdk-ble-hello-sensor --app-uri https://github.com/cypresssemiconductorco/mtb-example-btsdk-ble-hello-sensor --app-commit latest-v3.X --cypress-tools C:/Infineon/Tools/ModusToolbox/tools_2.4 --target-dir C:/Work/mtw --user-app-name LE_Hello_Sensor --output-for-machine --use-modus-shell
==============================================================================
= Cloning 'mtb-example-btsdk-ble-hello-sensor' =
==============================================================================
Cloning https://github.com/cypresssemiconductorco/mtb-example-btsdk-ble-hello-sensor into C:/Work/mtw directory...
env git clone --progress --origin cypress https://github.com/cypresssemiconductorco/mtb-example-btsdk-ble-hello-sensor LE_Hello_Sensor
Cloning into 'LE_Hello_Sensor'...
remote: Enumerating objects: 63, done.
remote: Counting objects: 100% (63/63), done.
remote: Compressing objects: 100% (25/25), done.
remote: Total 63 (delta 30), reused 60 (delta 30), pack-reused 0
Receiving objects: 100% (63/63), 49.76 KiB | 4.98 MiB/s, done.
Resolving deltas: 100% (30/30), done.
Checking out latest-v3.X...
env git checkout --progress latest-v3.X
Note: switching to 'latest-v3.X'.
You are in 'detached HEAD' state. You can look around, make experimental
changes and commit them, and you can discard any commits you make in this
state without impacting any branches by switching back to a branch.
If you want to create a new branch to retain commits you create, you may
do so (now or later) by using -c with the switch command. Example:
git switch -c <new-branch-name>
Or undo this operation with:
git switch -
Turn off this advice by setting config variable advice.detachedHead to false
HEAD is now at 9a3cc26 Upload mtb-example-btsdk-ble-hello-sensor 3.1.0.17479
==============================================================================
= Creating "TARGET_CYW920706WCDEVAL.mtb" file(s) =
==============================================================================
C:/Work/mtw/LE_Hello_Sensor/deps/TARGET_CYW920706WCDEVAL.mtb was added
C:/Work/mtw/LE_Hello_Sensor/deps/TARGET_CYW920819EVB-02.mtb was removed
==============================================================================
= Updating Makefile for "LE_Hello_Sensor" =
==============================================================================
==============================================================================
= Applying the Latest Version Locking for "LE_Hello_Sensor" =
==============================================================================
C:/Work/mtw/LE_Hello_Sensor/deps/TARGET_CYW920706WCDEVAL.mtb was updated
==============================================================================
= Getting Dependencies for "LE_Hello_Sensor" =
==============================================================================
C:/Infineon/Tools/ModusToolbox/tools_2.4/modus-shell/bin/make.exe getlibs CY_TOOLS_PATHS=C:/Infineon/Tools/ModusToolbox/tools_2.4
==============================================================================
= Importing libraries =
==============================================================================
Git is git version 2.33.0, found at /usr/bin/git
Resolving dependencies...
Checking if remote manifest is accessible...
Getting manifests from remote server...
Processing super-manifest https://github.com/cypresssemiconductorco/mtb-super-manifest/raw/v2.X/mtb-super-manifest-fv2.xml...
Successfully acquired the information.
C:/Work/mtw/LE_Hello_Sensor/libs/20706A2.mtb was added
C:/Work/mtw/LE_Hello_Sensor/libs/btsdk-common.mtb was added
C:/Work/mtw/LE_Hello_Sensor/libs/btsdk-include.mtb was added
C:/Work/mtw/LE_Hello_Sensor/libs/btsdk-tools.mtb was added
C:/Work/mtw/LE_Hello_Sensor/libs/btsdk-utils.mtb was added
C:/Work/mtw/LE_Hello_Sensor/libs/core-make.mtb was added
Dependencies resolved.
Searching application directory (.mtb)...
Found 10 .mtb file(s)
Processing file "C:/Work/mtw/LE_Hello_Sensor/deps/TARGET_CYW920706WCDEVAL.mtb"
fatal: loose object 4ce767e209cefd1bcbf785e0c2f2e5d4a6b184ee (stored in ./objects/4c/e767e209cefd1bcbf785e0c2f2e5d4a6b184ee) is corrupt
error: Could not fetch origin
ERROR: Unable to checkout "TARGET_CYW920706WCDEVAL". This is not a valid git repository.
==============================================================================
ERROR: --ABORTING--
: Script : C:/Infineon/Tools/ModusToolbox/tools_2.4/make/getlibs.bash
: Bash path : /usr/bin/bash
: Bash version: 4.4.12(3)-release
: Exit code : 1
: Call stack : trap_exit error perform_git process_mtb extract_data find_mtbs main
fatal: failed to copy file to '../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYW920706WCDEVAL/release-v3.1.0/.git/objects/00/1ce47243711f9148cc2ae167ddd2f0c8ac9cc0': Permission denied
make: *** [C:/Infineon/Tools/ModusToolbox/tools_2.4/make/getlibs.mk:121: getlibs] Error 1
Project "LE_Hello_Sensor" failed to create.
"make getlibs" failed.
Failed to create and export "LE_Hello_Sensor" application.
Solved! Go to Solution.
- Labels:
-
ModusToolbox Bluetooth SDK
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @AlenAn14 ,
> 1. Delete the folder in the path 'mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYW920706WCDEVAL'
I tried that, but got the same error.
> 2. If the above does not work, then, If its not too inconvenient for you, can you please uninstall and then install ModusToolbox in the default installation directory that is mentioned in the installer
Actually, C:/Infineon/Tools/ is the installation directory that was mentioned in the installer. I did not modify it! I just used "install for all users" option and did not modify anything except "mtw" directory location. And I set the environment variable afterwards, as it was suggested by the IDE.
However, I got it working now. I did the following:
- Uninstall Modus Toolbox
- Uninstall all drivers related to it
- Delete environment variable
- Reboot the PC
- Install Modus Toolbox without admin privileges, just for my user, using proposed paths - I used custom installation and unselected 2 options that require admin rights; since I have old WICED Studio installed with all drivers, it is not a problem
Now I'm able to generate a project, build and flash it. Although there're some errors or warnings during generation - please see attached log, - it gets generated anyway. So we can close this ticket.
Best regards,
Konstantin