Hello Infineon support team.
We are evaluating a sample application "Audio_Headset_and_Speaker" using CYW920721B2EVK-02.
<Board configuration>
-CYW9BTAUDIO2(J9) <-- Mic
-CYW9BTAUDIO2(J10) --> Headphone
-CYW9BTAUDIO2(J6 position)
short: 9-10, 11-12
open: 1~9
<Test Environment>
MIC/Headphone <--> CYW920721B2EVK-02 <--BT Connection--> pair device(mobile phone A) <--Calling--> mobile phone B
Now we are facing following phenomenon during calling.
- The headphone output works file.
- However, No voice output from mobile phone B. We suspected the mic input does not work well.
■Questions
1) Are the mic/J9 connection and J6 configuration is correct?
2) To enable line input path for the mic, we guess some registers of audio codec "CS47L35" need to configure.
Ex) "R768(0x0300) Input_Enables" register .
Does this sample application configure those registers?
Thanks,
Tayo
Solved! Go to Solution.
Hi,
Could you please check by shorting below jumpers.
J19 :1-2,
J6: 3-4, 5-6, 7-8, 9-10
When you get the phone call, you may be able to respond through the J10 itself.
Thanks,
-Dheeraj.P.K
Hi,
Could you please check by shorting below jumpers.
J19 :1-2,
J6: 3-4, 5-6, 7-8, 9-10
When you get the phone call, you may be able to respond through the J10 itself.
Thanks,
-Dheeraj.P.K
Hello Dheeraj-san
Thank you for your comment.
We will retest with the board configuration.
Thanks,
Tayo