- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am really struggling to get i2s microphone to stream to a2dp,
I've looked everywhere including watch example to try get this to work but to no avail.
I am using a board CYW20706 and have a microphone connected to it via i2s (it is a 24bit microphone).
Do the gpio pins need to be set? or am I missing a library such as CYW9BT_audio in the watch example for this to work?
I have configured the board as the i2s slave and a2dp source and the microphone as the master using wiced_audio_start();
Is there anything else I can try to make this work?
I've looked a this link too and tried other boards such as 20719 and 20819, all seem to not work.
At this point, any help would be greatly appreciated. I've been stuck with this problem for the last 2months 😞
Thankyou so much in advance!
Solved! Go to Solution.
- Labels:
-
ModusToolbox Bluetooth SDK
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
My apologies, I got confused. Yes it can be configured as i2s master and slave both.
I just confirmed internally that I2S input on watch app supports on 20721 based platforms only.
CYW20721B2 is the latest audio solution by Cypress which supports most of the audio features. CYW20706 supports some of the audio features, but not all. CYW20719 and 20819 also supports basic A2DP source, AVRCP features demonstrated in watch demo example. Apart from that, no extra or advanced audio functionalities are supported by these chips.
To get access to CYW20721 chip/eval board, you will need to contact Cypress Sales team or FAE. I will provide you specific details over personal message.