Bluetooth SIG has announced some security notices on the following URL.
Please let me know if CYW20819 has the issue related to CVE-2020-26555 and CVE-2020-26558 or not.
If yes, I'd like to get the patches or workaround.
Thanks
Solved! Go to Solution.
Hi,
Regarding CVE-2020-26555, The suggestion from the SIG is,
"The Bluetooth SIG is recommending that potentially vulnerable devices not initiate or accept connections from remote devices claiming the same BD_ADDR as the local device. The Bluetooth SIG continues to recommend that devices use Secure Simple Pairing or BR/EDR Secure Connections to avoid known vulnerabilities with legacy BR/EDR pairing."
So here, customers can implement the logic in their applications to reject the legacy pairing PIN request when it found the remote BD Address is the same as local.
Thanks,
-Dheeraj
Hi,
We will check internally and get back to you.
Thanks,
-Dheeraj
Can I have some update?
I need the information about whether CYW20819 has these vulnerabilities or not, and if yes how to fix it.
Do you have an estimated time-frame of when you expect to get these information?
Regards
Hi,
Regarding CVE-2020-26555, The suggestion from the SIG is,
"The Bluetooth SIG is recommending that potentially vulnerable devices not initiate or accept connections from remote devices claiming the same BD_ADDR as the local device. The Bluetooth SIG continues to recommend that devices use Secure Simple Pairing or BR/EDR Secure Connections to avoid known vulnerabilities with legacy BR/EDR pairing."
So here, customers can implement the logic in their applications to reject the legacy pairing PIN request when it found the remote BD Address is the same as local.
Thanks,
-Dheeraj
Please let me know about CVE-2020-26558 too.
Thanks
Hi,
Regarding CVE-2020-26558.
The fix should be done in both the host and controller and it is partially completed and released in the latest SDK. The complete fix for the vulnerability will be available in the upcoming BTSDK released by July End.
Thanks,
-Dheeraj