https://community.cypress.com/t5/ModusToolbox-Bluetooth-SDK/CYW20819-LPM-and-UART/m-p/93362
On my previous thread, I got the following message.
"Please note that PUART hardware flow control has some in the current SDK. Our dev team has already fixed the issue, and the fix will be available on the next SDK."
Could I have the information whether the issue is fixed on SDK v2.9?
It seems that Hardware flow is disabled by LPM (ePDS) even if I use SDK v2.9.
Solved! Go to Solution.
Hi,
I believe, the issue is fixed.
May I know on which kit are you testing? If it is CYW920819EVB-02 kit, then please note that the the PUART’s RTS on the USB-Serial chip is not connected to any of the CYW20819 GPIOs. Low power mode should not disable flow control.
Thanks,
-Dheeraj
Hi,
I believe, the issue is fixed.
May I know on which kit are you testing? If it is CYW920819EVB-02 kit, then please note that the the PUART’s RTS on the USB-Serial chip is not connected to any of the CYW20819 GPIOs. Low power mode should not disable flow control.
Thanks,
-Dheeraj
I tested this with our evaluation board that support UART hardware flow control (RTS/CTS).
It seems that the behavior about LPM is not changed. When waking-up from LPM, UART flow remains disabled.
By re-initializing in wake-up callback, UART flow control is re-initialized.
void lpm_post_sleep_callback(wiced_bool_t restore_configuration){
if(restore_configuration){
uart_reinit();
wiced_auth_chip_reinit();
}
return;
}
void uart_reinit(void){
wiced_hal_gpio_select_function(WICED_P00, WICED_UART_2_RTS);
wiced_hal_gpio_select_function(WICED_P10, WICED_UART_2_CTS);
wiced_hal_puart_flow_on();
CRITICAL_REGION_ENTER();
bt_app.flag_uart_reinit = 1;
CRITICAL_REGION_EXIT();
return;
}
Please show me whether next SDK will support the functionality to restore UART flow control automatically or we should restore it manually in wake-up callback function.
But I am facing the issue that there are the case that the callback is not generated........
As I said in the previous thread, we have to call the platform init in the wake up call back. This is expected, not an issue
Please check https://www.cypress.com/documentation/application-notes/an225270-cyw208xx-ble-low-power-guidelines
Thanks,
-Dheeraj