- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @AnjanaM_61
I am trying to use this OPP server application https://github.com/Infineon/mtb-example-btsdk-rfcomm-opp-server for CYW920819-EVB02. I am able to load application onto the board and then use ClientControl application to discover devices. From my other Bluetooth device, I pair to the OPP server on the evaluation board and can send .vcf files. However, I am not able to send .txt or .jpg image etc.
Even though it is stated in README that it is possible: The Object Push Profile server is used to receive object files (e.g vCard, Image, Text, etc.). Send object files from an OPP client (mobile phone or PC).
I have tried using 2 different devices to send jpg but the OPP server loading bar in Client Control will just remain at 0.
May I know why is this so?
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
Yes, I am using the latest SDK and ModusToolbox version.
Just to let you know I have also tried to send png image. For png it shows 100% transferred successful but when opening the image file it is corrupted. I tried with different png images so doesn’t seem to be problem with image.
i also retry using jpeg and it sometimes show 100% BUT the actual file when opening using text editor it is absolutely empty (0 byte)