Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Bluetooth SDK Forum Discussions

YR1
Level 2
Level 2
5 questions asked 5 replies posted First solution authored
A2DP_SRC_INCLUDED := 0
A2DP_SNK_INCLUDED ?= 1
关闭source 打开sink样例直接构建失败.
 

wiced_app.c:63:10: fatal error: a2dp_sink.h: No such file or directory
63 | #include "a2dp_sink.h"
| ^~~~~~~~~~~~~
compilation terminated.
Compiling ../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common/spar_setup.c -DWICED_BT_TRACE_ENABLE -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT_UART=1 -DSLEEP_SUPPORTED=0 -DCOEX_SUPPORTED=0 -DWICED_HCI_TRANSPORT=1 -DWICED_APP_AUDIO_SNK_INCLUDED -DA2DP_SINK_ENABLE_CONTENT_PROTECTION -DWICED_A2DP_EXT_CODEC=0 -DWICED_APP_AUDIO_RC_TG_INCLUDED -DCATEGORY_2_PASSTROUGH -DWICED_APP_AUDIO_RC_CT_INCLUDED -DMAX_CONNECTED_RCC_DEVICES=1 -DWICED_APP_LE_INCLUDED -DWICED_APP_LE_PERIPHERAL_CLIENT_INCLUDED -DWICED_APP_ANCS_INCLUDED -DWICED_APP_AMS_INCLUDED -DWICED_APP_TEST_INCLUDED -DWICED_HCI_TRANSPORT_UART=1 -DWICED_HCI_TRANSPORT_SPI=2 -DWICED_HCI_TRANSPORT=1 -DHCI_UART_MAX_BAUD=4000000 -DHCI_UART_DEFAULT_BAUD=3000000 -DSS_LOCATION=0 -DVS_LOCATION=4096 -DDS_LOCATION=16384 -DDS2_LOCATION=270336 -DCYW20706A2=1 -DBCM20706A2=1 -DBCM20706=1 -DCYW20706=1 -DCHIP=20706 -DAPP_CHIP=20706 -DOTA_CHIP=20706 -DCHIP_REV_A_20706A2=1 -DBCM20703 -DBUILDCFG -DCOMPILER_ARM -DSPAR_APP_SETUP=application_setup -D__TARGET_CPU_CORTEX_M3 -D__ARMCC_VERSION=400677 -DPLATFORM='"CYW920706WCDEVAL"' -DCYW920706WCDEVAL -DCY_PATCH_ENTRIES_BASE=123 -DWICED_SDK_MAJOR_VER=4 -DWICED_SDK_MINOR_VER=1 -DWICED_SDK_REV_NUMBER=3 -DWICED_SDK_BUILD_NUMBER=59500 -DSPAR_CRT_SETUP=spar_crt_setup -DCOMPONENT_20706A2 -DCOMPONENT_MW_20706A2 -DCOMPONENT_MW_BTSDK_AUDIO -DCOMPONENT_MW_BTSDK_COMMON -DCOMPONENT_MW_BTSDK_HOST_APPS_BT_BLE -DCOMPONENT_MW_BTSDK_INCLUDE -DCOMPONENT_MW_BTSDK_OTA -DCOMPONENT_MW_BTSDK_PAN -DCOMPONENT_MW_BTSDK_PEER_APPS_BLE -DCOMPONENT_MW_BTSDK_PEER_APPS_OTA -DCOMPONENT_MW_BTSDK_TOOLS -DCOMPONENT_MW_BTSDK_UTILS -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_TARGET_CYW920706WCDEVAL -DCOMPONENT_SOFTFP -DCOMPONENT_a2dp_sink_profile -DCOMPONENT_ams -DCOMPONENT_ancs -DCOMPONENT_avrc_controller -DCOMPONENT_avrc_target -DCOMPONENT_bsp_design_modus -DCOMPONENT_btstack_v1 -DCY_SUPPORTS_DEVICE_VALIDATION -DCYW20706UA2KFFB4G -I. -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2 -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/WICED/common -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/hal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/internal -I../mtb_shared/wiced_btsdk/dev-kit/baselib/20706A2/release-v4.1.3/COMPONENT_20706A2/include/stack -I../mtb_shared/wiced_btsdk/dev-kit/bsp/TARGET_CYW920706WCDEVAL/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/btsdk-include/release-v4.1.3 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_a2dp_sink_profile -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_ams -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_ams/btstack_v1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_ams/btstack_v3 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_ancs -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_ancs/btstack_v1 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_ancs/btstack_v3 -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_avrc_controller -I../mtb_shared/wiced_btsdk/dev-kit/libraries/btsdk-audio/release-v3.3.0/COMPONENT_avrc_target -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v3.3.0 -I../mtb_shared/wiced_btsdk/tools/btsdk-host-apps-bt-ble/release-v3.3.0/include -I./COMPONENT_btstack_v1 -I./COMPONENT_btstack_v1/GeneratedSource
make[1]: *** [../mtb_shared/core-make/release-v1.9.1/make/core/build.mk:377: C:/Users/46996/mtw/Audio_Watch_1/build/CYW920706WCDEVAL/Debug/wiced_app.o] Error 1
make[1]: *** Waiting for unfinished jobs....
make: *** [../mtb_shared/core-make/release-v1.9.1/make/core/main.mk:434: secondstage_build] Error 2
"C:/Infineon/Tools/ModusToolbox/tools_3.0/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_MAKE_IDE_VERSION=3.0 CY_IDE_TOOLS_DIR=C:/Infineon/Tools/ModusToolbox/tools_3.0 -j8 all" terminated with exit code 2. Build might be incomplete.

11:40:43 Build Failed. 4 errors, 0 warnings. (took 14s.637ms)

 

0 Likes
1 Solution
Owen_Zhang123
Moderator
Moderator
Moderator
500 solutions authored 250 sign-ins 1000 replies posted

watch的demo里只有A2DP Source的功能,没有A2DP Sink,如果你要使用A2DP sink,可以参考A2DP_Sink的demo,需要添加一下额外的库。

CYW20706的资源应该是无法同时跑A2DP Sink和souce的。

View solution in original post

0 Likes
4 Replies
Owen_Zhang123
Moderator
Moderator
Moderator
500 solutions authored 250 sign-ins 1000 replies posted

请问你直接编译的是modus上的工程失败?是否做了改动?

使用的SDK版本是多少?

0 Likes
YR1
Level 2
Level 2
5 questions asked 5 replies posted First solution authored
makefile修改了
A2DP_SRC_INCLUDED := 0
A2DP_SNK_INCLUDED ?= 1
 
<version>4.1.3.59500</version>
0 Likes
Owen_Zhang123
Moderator
Moderator
Moderator
500 solutions authored 250 sign-ins 1000 replies posted

watch的demo里只有A2DP Source的功能,没有A2DP Sink,如果你要使用A2DP sink,可以参考A2DP_Sink的demo,需要添加一下额外的库。

CYW20706的资源应该是无法同时跑A2DP Sink和souce的。

0 Likes

没用的代码可以清理下吗? 

https://github.com/Infineon/mtb-example-btsdk-audio-watch/blob/master/makefile

A2DP_SNK_INCLUDED ?= 0

开关放在这容易歧义

代码里也有很多SINK的东西

0 Likes
This widget could not be displayed.