Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PCB layout tips for low side gate drivers with OCP

PCB layout tips for low side gate drivers with OCP

wchu1
Employee
Employee
First like received Welcome! First solution authored

Our 1ED44173/5/6 are the new low side gate driver ICs that integrate over-current protection (OCP), FAULT status output and enable function. This high integration level is excellent for the digitally controlled Power Factor Correction (PFC) applications with boost topology and ground reference switching.

In PFC applications, shunts are used to sense power switch current or DC bus current. The shunt’s location is different depending on the control methodology chosen. In Figure 1, Example 1, for example, the shunt is located between the IGBT emitter and system ground in order to sense the power switch’s current when the controller implements peak current control or current balance control in the interleaved PFC applications.

By contrast, Figure 1, Example 2 shows the shunt located between the system ground and negative DC bus minus rail in order to sense DC bus current. This configuration is popularly used in the average current mode control, and the digital controller can calculate input power based on average current and DC bus feedback.

Figure-1.PNG_1869599209.pngFigure 1: Two different types of low side gate drivers with OCP: 1ED44176N01F (Example 1) has positive current sense to meet the first shunt configuration, while 1ED44173/5N01B (Example 2) have the negative current sense to meet the second shunt configuration

Applications in residential air conditioning


In today’s residential air conditioning (RAC) applications with digitally controlled PFC, the controller uses the power feedback signal to implement the adaptive DC bus voltage control. This allows lower losses at light loads when a lower DC bus is used and switches over to a full DC bus when a full load is required.

Because of the different shunt configurations, Infineon has designed two different types of the low side gate drivers with OCP: 1ED44176N01F (Figure 1, Example 1), as well as 1ED44173N01B and 1ED44175N01B (Figure 1, Example 2). The former has the positive current sense meet the first shunt configuration, while the latter two have the negative current sense meet the second shunt configuration. The 1ED44175N01B is targeted for use with IGBTs, while the 1ED44173N01B is targeted for use with MOSFETs.

Figure-2.PNG_1534170322.pngFigure 2: The table shows the differences between 1ED44173/5/6
 
PCB layout is always a challenge in high-current, fast-switching circuits like PFC. A good PCB layout provides proper device operation and design robustness. Improper components or placement may cause erratic switching, excessive voltage ringing, or circuit latch-up.
 
The best PCB layout tips for gate driver ICs:

  1. When employing an RC filter circuit between micro-controllers and the gate drivers, keep the wiring of the input as short as possible (less than 2-3 cm).

  2. EN/ FLT output is an open-drain output, so it needs to be pulled up to a 5 V or 3.3 V logic power supply with a pull-up resistor. When positioning, place the RC filter close to gate driver.

  3. In order to prevent false triggering in over current protection, the RC filter wiring between OCP and ground should be as short as possible.

  4. Mount each capacitor as close to the pins of the gate drivers as possible.

  5. Connect the ground pin of the microcontroller directly to the COM pin (1ED44173/5N01B).

  6. Connect the gate output return to the COM and connect the ground pin of the micro-controller to the VSS logic ground pin (1ED44176N01F) This can prevent noise coupling of the logic input pins from the driver output loop.

Let’s look at the effect the right layout can have. The following example shows the case of a circuit (Figure 3) and layout implementation (Figure 4) for the 1ED44175N01B and a TO-247 IGBT (e.g. IKW40N65WR5). With this design, it is possible to reduce the PCB trace loop area and inductance.

FIgure-3.PNG_71503822.pngFigure 3: Circuit diagram with 1ED44175N01B.

Figure-4.PNG_929454831.pngFigure 4: Layout of the above circuit.


Factors leading to the reduction of PCB trace loop area and inductance:


  • Placing the 1ED44175N01B close to the IGBT gate and emitter.
  • Placing the decoupling capacitor (C3) directly at the VCC and COM pins.
  • Placing the filter capacitors (C1 and C4) and fault clear time programming capacitor (C2) close to the pins.
  • Locating ground planes directly above or beneath the 1ED44175N01B, which can reduce trace inductance.

Additionally, a ground plane connected to the COM helps as a radiated noise shield and provides some heat sinking for power dissipated within the device.

Following these layout tips eliminates common noise coupling issues which can cause mis-operation and reduce the initial design time.

To find out more about the 1ED44173/5/6 products, their evaluation boards, and online simulations (IFX designer), visit their respective product pages below:

0 Likes
958 Views
Authors