Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

NOR: Infineon XMC4800 Relax EtherCAT Kit now features Infineon NOR Flash memory S25FL064L

NOR: Infineon XMC4800 Relax EtherCAT Kit now features Infineon NOR Flash memory S25FL064L

BushraH_91
Moderator
Moderator
Moderator
750 replies posted 50 likes received 250 solutions authored

                          

BushraH_91_0-1622567779025.jpeg

Infineon’s evaluation kit for the XMC4800-F144 microcontroller (XMC4800 Relax EtherCAT Kit) has recently undergone a major update to replace a competitor’s Flash memory with an Infineon quad SPI Flash memory, namely S25FL064LABMFI01x. This Flash Memory family meets the high standards of reliability and performance required by industrial systems.

And you may be asking what features does this new evaluation kit have? It’s a great question, and below you can find that list as well as taking the link to find more details and purchase a kit.

Summary of Features:

- XMC4800-F144 Microcontroller based on ARM® Cortex®-M4@144MHZ, integrated EtherCAT® Slave Controller, 2MB Flash and 352KB RAM

- On-Board Debugger

- Power over USB

- ESD and reverse current protection

- 2 x user button and 2 x user LED

- Arduino hardware compatible 3.3V pinout

- Real Time Clock crystal

- Quad SPI Flash

- microSD Card Slot

- Ethernet PHY and RJ45 Jack

- CAN node

- EtherCAT® node

Please refer to following link for more information and to buy online:

Infineon XMC4800 Relax EtherCAT Kit

 

0 Likes
235 Views
Authors